How to Measure Signal Frequency by Using the Camera Sensor Interface of an i.MX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Measure Signal Frequency by Using the Camera Sensor Interface of an i.MX

How to Measure Signal Frequency by Using the Camera Sensor Interface of an i.MX

This describes how to perform frequency measurements of an external signal by using the Camera Sensor Interface (CSI) of an i.MX21/25/35 processor.

  1. Principle:

A way to measure the frequency of a digital signal is to count the number of received rising or falling edges during a known amount of time.

The CSI embeds a 16-bit frame counter. When programmed in non-gated clock mode, this counter increases at any rising edge on the VSYNC signal.

Other signals of this interface could be ignored such: MCLK, PIXEL_CLK, HSYNC, DATA.

  1. Software example for the i.MX25:

void CSI_init(void){

      unsigned int tmp_value = 0;

      /* It assumes that the VSYNC I/O is set to CSI mode */

      /* Disable IPG_PER_CSI to save power consumption */

      *((unsigned int *) CCM_CGR0) &= ~(0x1<<0);

      /* HCLK_CSI and IPG_CLK_CSI should be enabled. */

      *((unsigned int *) CCM_CGR0) |= (0x1<<18);

      *((unsigned int *) CCM_CGR1) |= (0x1<<4);

      /* Configuration of CSI_CSICR1 in non-gated clock mode */

      tmp_value = 0;

      tmp_value |= (1<<8);    // sync FIFO clear

      tmp_value |= (1<<30);   // ext vsync enable

      *((unsigned int *) CSI_CSICR1) = tmp_value;

      // Reset frame counter

      *((unsigned int *) CSI_CSICR3) |= (1<<15);

}

Then, every T seconds, the software has to read the register CSI_CSICR3. The 16-bit size field from bit 16 shows the current value of the frame counter (FRMCNT).

This regular or irregular read could be done based on a GPT to have a known time reference.

It is easy to calculate the frequency of the signal: Frequency = FRMCNT / T (Hz).

At any time, the frame counter can be reset thanks to the bit 15 of the register CSI_CSICR3.

NOTES:

  • MCLK does not need to be enabled.
  • The input frequency should not be higher than what can electrically support the VSYNC input.
  • Please, refer to each i.MX datasheet for more information.


ラベル(1)
タグ(3)
評価なし
バージョン履歴
最終更新日:
‎11-22-2012 09:47 AM
更新者: