| Audio, from a file | gst-launch filesrc location=test.wav ! wavparse ! mfw_mp3encoder ! filesink location=output.mp3 |
| Audio Recording | gst-launch alsasrc num-buffers=$NUMBER blocksize=$SIZE ! mfw_mp3encoder ! filesink location=output.mp3 # where # duration = $NUMBER*$SIZE*8 / (samplerate *channel *bitwidth) # Example: 60 seconds recording # gst-launch alsasrc num-buffers=240 blocksize=44100 ! mfw_mp3encoder ! filesink location=output.mp3 # # To verify that is correct, do a normal audio playback gst-launch filesrc location=output.mp3 typefind=true ! beepdec ! audioconvert ! 'audio/x-raw-int,channels=2' ! alsasink |
| Video, from a test source | gst-launch videotestsrc ! queue ! vpuenc ! matroskamux ! filesink location=./test.avi |
| Video, from a file | gst-launch filesrc location=sample.yuv blocksize=$BLOCK_SIZE ! 'video/x-raw-yuv,format=(fourcc)I420, width=$WIDTH, height=$HEIGHT, framerate=(fraction)30/1' ! vpuenc codec=$CODEC ! matroskamux ! filesink location=output.mkv sync=false # where # BLOCK_SIZE = WIDTH * HEIGHT * 1.5 # CODEC = 0(MPEG4), 5(H263), 6(H264) or 12(MJPG). # # For example, encoding a CIF raw file gst-launch filesrc location=sample.yuv blocksize=152064 ! 'video/x-raw-yuv,format=(fourcc)I420, width=352, height=288, framerate=(fraction)30/1' ! vpuenc codec=0 ! matroskamux ! filesink location=sample.mkv sync=false |
| Video, from Web camera | # when the web cam is connected, the device node /dev/video0 should be present. In order to test the camera, without encoding gst-launch v4l2src ! mfw_v4lsink # in recording, run: # # # where sync=false indicates filesink to to use a clock sync # # In case a specific width/height is needed, just add the filter caps gst-launch v4l2src num-buffers=-1 ! 'video/x-raw-yuv,format=(fourcc)I420, width=352, height=288, framerate=(fraction)30/1' ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false # # In case you want to see in the screen what the camera is capturing, add a tee element # gst-launch v4l2src num-buffers=-1 ! tee name=t ! queue ! mfw_v4lsink t. ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false |
| Video, from Parallel/MIPI camera | # The camera driver needs to be loaded before executing the pipeline, refer to the BSP document to see which driver to load # MIPI (J5 port): modprobe ov5640_camera_mipi modprobe mxc_v4l2_capture
# Parallel (J9 port): modprobe ov5642_camera modprobe mxc_v4l2_capture
gst-launch mfw_v4lsrc ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false
# Do a 'gst-inspect mfw_v4lsrc' or 'gst-inspect vpuenc' to see other possible settings (resolution, fps, codec, etc.) |
Hi,
I'm using boundary device sabreLite and when trying to record video from ov5640 mipi,Its show some error.
command:
gst-launch mfw_v4lsrc ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false
output msg:
MFW_GST_V4LSRC_PLUGIN 3.0.8 build on Sep 23 2014 05:49:17.
Setting pipeline to PAUSED ...
[INFO] Product Info: i.MX6Q/D/S
vpuenc versions :smileyhappy:
plugin: 3.0.8
wrapper: 1.0.38(VPUWRAPPER_ARM_LINUX Build on Sep 23 2014 05:42:43)
vpulib: 5.4.15
firmware: 2.3.10.40778
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
ERROR: from element /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0: Internal data flow error.
Additional debug info:
gstbasesrc.c(2625): gst_base_src_loop (): /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0:
streaming task paused, reason error (-5)
Execution ended after 9999770667 ns.
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...
-----------------------------------------------------------------------------------------------------------------------------------
But when i include capture-mode
gst-launch mfw_v4lsrc capture-mode=4 ! queue ! vpuenc codec=0 ! matroskamux ! filesink location=output.mkv sync=false
ls -al
-rwxr-xr-x 1 root root 10476028 Oct 13 2014 output.mkv
When i try to open in vlc, its showing like a image(photo) not a running video.
Please hep me out.
-Sridhar
Strange. Do you see the same behavior using gplay to reproduced the recorded video? gplay runs on target.
Is there command for Video/Audio recording? Thank you.