Config Tools for i.MX v25.09 Now Available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Config Tools for i.MX v25.09 Now Available

Config Tools for i.MX v25.09 Now Available

We are pleased to announce that Config Tools for i.MX v25.09 are now available.

Downloads & links

Release Notes

Full details on the release (features, known issues...)

• The Release Notes format is updated from plain text to markdown.
• The newly generated configuration includes the default NXP copyright notice and is licensed under the
BSD-3-Clause license.
DDR tool
– ODT and Driver Strength Updates for LP4/LP5 on i.MX 943 and i.MX 95
– Improved DRAM Configuration for i. MX 9x devices
– Multicore support is enabled for DDR tests on i.MX 943 and i.MX 95
– Linux support for the DDR tool
– Vref DQ Setting now available in the GUI
– Board-agnostic SM Support for i.MX 943 and i.MX 95
– DDR part number entry is supported in the GUI
– Enhanced logging from the target application
– Stress test repetition option is enabled
– Updated ODT shmoo scenario values on i.MX 943 and i.MX 95
– Support for SNPS FW and PHY Init 2024.09 SP2 on i.MX 943 and i.MX 95
– AHAB image update to align with BSP for CES parts on i.MX 943 and i.MX 95
– New configuration support for 15x15 on i.MX 943
– Improved bus configuration for single-channel setups
– LP4/LP5 CS signal configuration now exposed in the GUI for i.MX 943 and i.MX 95
Clocks
– Supported input frequency setting
System Manager
– Initial version of the tool

无评分
版本历史
最后更新:
‎09-30-2025 10:42 AM
更新人: