Building External Kernel Modules for Linux 6.12: Cross-Compilation Guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building External Kernel Modules for Linux 6.12: Cross-Compilation Guide

Building External Kernel Modules for Linux 6.12: Cross-Compilation Guide

Hello! In this post, we’ll cross-compile a kernel module for Linux 6.12.   

This can be done either using a standalone kernel or a Yocto-built kernel. 

 

Requirements: 

  • A compiled Linux kernel 6.12. 
  • A board running the same kernel version (Linux 6.12 in this case). 
  • A cross-compiler toolchain. 

 

This process applies to any i.MX processor, including i.MX8, i.MX8M, i.MX8MM, i.MX8MN, i.MX8MP, i.MX93, i.MX91, i.MX95, as well as the i.MX6 and i.MX7 families. 

 

Step 1: Compile the Linux Kernel and get the Toolchain 

 

First, you need to compile the Linux kernel (6.12 in this case).   

You can do this in a standalone environment or using Yocto. 

  

If you are using a Standalone environment, please refer to the Chapter 4.5.12 How to build U-Boot and Kernel in standalone environment of i.MX Linux User's Guide. 

Also, in that document section, you will see how to obtain the cross-compiler toolchain. 

 

NOTE: To get the toolchain you need use Yocto at least once (for more information please refer to i.MX Yocto Project User's Guide 

$ DISTRO=fsl-imx-xwayland MACHINE=Target-Machine bitbake core-image-minimal -c populate_sdk 

 

At the end of the building, you can install your toolchain populated under: 

 

yocto-bsp/build/tmp/deploy/sdk  

 

There you will find a file called: 

 

fsl-imx-wayland-glibc-x86_64-imx-image-core-armv8a-your-machine-name-toolchain-6.12-walnascar.sh 

 

Execute with: 

$ sudo ./fsl-imx-wayland-glibc-x86_64-imx-image-core-armv8a-your-machine-name-toolchain-6.12-walnascar.sh  

 

If you use the default installation, you will have your toolchain under /opt in your host machine. 

 

 

(If you will use the compiled kernel from Yocto, you can avoid below step) 

Download Standalone Kernel source by cloning with: 

$ git clone https://github.com/nxp-imx/linux-imx -b lf-6.12.y 
$ cd linux-imx 

 

To build the kernel in the standalone environment for i.MX 6 and i.MX 7, execute the following commands: 

 

$ make imx_v7_defconfig  
$ Make

 

To build the kernel in the standalone environment for i.MX 8 and i.MX 9, execute the following commands: 

$ make imx_v8_defconfig  
$ make 

 

The full kernel compilation is required to generate headers and symbol files required for external module compilation, even if you don't plan to boot this kernel directly. 

 

 

Step 2: Write a simple Kernel Module to test 

 

Now that your kernel is compiled, you can write a basic kernel module for testing. 

 

Create a new directory. It will have our hello.c and Makefile. 

 

We will create the file hello.c: 

#include <linux/init.h> 
#include <linux/module.h> 
#include <linux/kernel.h> 

MODULE_LICENSE("GPL"); 
MODULE_AUTHOR("Salas"); 
MODULE_DESCRIPTION("A simple kernel module example for cross-compilation."); 
MODULE_VERSION("0.1"); 

static int __init hello_init(void) { 
    printk(KERN_INFO "Hello from the kernel module!\n"); 
    return 0; 
} 

static void __exit hello_exit(void) { 
    printk(KERN_INFO "Goodbye from the kernel module!\n"); 
} 

module_init(hello_init); 
module_exit(hello_exit); 

 

 

Then, create a basic Makefile to compile the modules: 

 

# Module name 
obj-m += hello.o 

# Build flags 
ldflags-y += --strip-debug 

# Kernel source directory (provided by Yocto) 
KERNEL_SRC ?= /path/to/your/compiled/kernel 

# Build target 
all: 
$(MAKE) -C $(KERNEL_SRC) M=$(PWD) modules 

# Clean target 
clean: 
$(MAKE) -C $(KERNEL_SRC) M=$(PWD) clean 

# Install target 
modules_install: 
$(MAKE) -C $(KERNEL_SRC) M=$(PWD) modules_install 

 

KERNEL_SRC should be your compiled kernel from your Yocto build:  

yocto-bsp/build/tmp/work/your-machine-poky-linux/linux-imx/6.12.20+git/build 

 

Or the Standalone :

path/to/linux-imx/ 

 

 

Step 3: Set the toolchain and compile the kernel module 

 

Finally, we can compile the kernel module. 

 

First, set the toolchain (in my case): 

$ source /opt/fsl-imx-wayland/6.12-walnascar/environment-setup-armv8a-poky-linux

 

Then, compile using the makefile: 

$ make 

 

f everything goes well, at final you will have the generated files: 

 

hello.ko 
hello.mod 
hello.mod.c 
hello.mod.o 
hello.o 
Makefile 
modules.order 
Module.symvers 

 

The one we need is the hello.ko (Kernel Object). 

 

We can check if the file was created correctly using: 

 

$ readelf -h hello.ko 
ELF Header: 
  Magic:   7f 45 4c 46 02 01 01 00 00 00 00 00 00 00 00 00  
  Class:                             ELF64 
  Data:                              2's complement, little endian 
  Version:                           1 (current) 
  OS/ABI:                            UNIX - System V 
  ABI Version:                       0 
  Type:                              REL (Relocatable file) 
  Machine:                           AArch64 
  Version:                           0x1 
  Entry point address:               0x0 
  Start of program headers:          0 (bytes into file) 
  Start of section headers:          33992 (bytes into file) 
  Flags:                             0x0 
  Size of this header:               64 (bytes) 
  Size of program headers:           0 (bytes) 
  Number of program headers:         0 
  Size of section headers:           64 (bytes) 
  Number of section headers:         41 
  Section header string table index: 40

 

We can see the Machine is AArch64 and the Type is a Relocatable file. 

 

 

Step 4: Running the Kernel Object/Module in the board 

 

Transfer the generated hello.ko file from your host machine to your board. 

 

Then, In your board you can run with: 

 

root@imx93evk:~# ls 
hello.ko 
root@imx93evk:~# insmod hello.ko  
root@imx93evk:~# dmesg | tail 
[ 5140.547447] Hello world from kernel! 
root@imx93evk:~# rmmod hello.ko  
root@imx93evk:~# dmesg | tail 
[ 5140.547447] Hello world from kernel! 
[ 5153.415215] Goodbye world from kernel! 

 

I hope this can helps to you. 

 

Best regards, 

Salas. 

No ratings
Version history
Last update:
‎07-11-2025 09:05 AM
Updated by: