The purpose of this document is to provide extended guidance for selection of compatible LPDDR4 memory devices that are supported by the Ara240 (aka Ara-2) processors. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the specific SoC requirement documents.
| SoC | Max Data bus width | Maximum density | Number of Interfaces | Assumed memory organization | Notes |
| Ara240 | 64-bit | 128Gb/16GB | 2 |
Dual rank, Dual channel device with 17-row addresses |
1 |
The validation process is an ongoing effort - regular updates of the table are expected.
| SoC | Density | Memory Vendor | Validated Memory Part# | Notes |
| Ara240 |
64Gb/(8GB) Total 128Gb/(16GB) (2 x 64Gb/8GB) |
Micron | - | |
|
64Gb/(8GB) Total 128Gb/(16GB) (2 x 64Gb/8GB)
|
FORESEE |
FLXC4008G-30 | 2 | |
|
16Gb/(2GB) Total: 32Gb/(4GB) (2 x 16Gb/2GB) |
Micron |
MT53E512M32D1ZW-046BAUT:B |
- | |
|
32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB)
|
Micron |
MT53E1G32D2NP-046 WT:B |
- | |
|
16Gb/(2GB) Total: 32Gb/(4GB) (2 x 16Gb/2GB) |
SK Hynix |
H54G46CYRQX053N |
- | |
|
32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB) |
SK Hynix |
H54G56CYRB-X247 421Y H54G56CYRB-X247 316A |
- | |
|
4Gb/(512MB) Total 8Gb/1GB (2 x 4Gb/1GB) |
SK Hynix |
H54G26AYRBX256 |
- | |
|
16Gb/(2GB) Total: 32Gb/(4GB) (2 x 16Gb/2GB) |
Samsung |
K4F6E3S4HB-KHCL |
- | |
|
32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB) |
ISSI |
IS43LQ32K01B |
2 | |
|
32Gb/(4GB) Total 64Gb/8GB (2 x 32Gb/4GB) |
Samsung |
K4UBE3D4AB-MGCL |
- |
|
|
8Gb/(1GB) Total 16Gb/2GB (2 x 8Gb/1GB)
|
Winbond |
2 |
Note: This device supports operation with LPDDR4 memories only. LPDDR4x operation is not supported.
Dual‑mode memories that support both LPDDR4 and LPDDR4x are allowed as long as the device can operate in LPDDR4 mode,
including using LPDDR4 I/O voltage levels and initialization sequences.
Note 1:
The numbers are based purely on the IP documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, SoC reference manual and on the JEDEC standards JESD209-4C (LPDDR4). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk.
Note 2:
The memory part number did not undergo full JEDEC verification however, it passed all functional testing items.
Note 3:
Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity.
Note 4:
All memory parts are in production unless stated otherwise. Checked June 2026
Note 5:
The processor does not support BYTE Mode (x8) memories.
Cross reference: