Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

The i.MX Android O8.0.0_1.0.0 GA release is now available from IMX_SW page. Overview -> BSP Updates and Releases -> Android 8.0.0 Oreo (O8.0.0_1.0.0, 4.9 kernel)

 

  • Files available:

#

Name

Description

1

android_O8.0.0_1.0.0_docs.tar.gz

i.MX Android O8.0.0_1.0.0 BSP Documentation

2

imx-o8.0.0_1.0.0_ga.tar.gz

i.MX Android O8.0.0_1.0.0 proprietary surce code for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite, i.MX6SX and i.MX7D

3


android_O8.0.0_1.0.0_image_6dqpsabreauto.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite

4

android_O8.0.0_1.0.0_image_6dqpsabresd.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite.

5

android_O8.0.0_1.0.0_image_6slevk.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - i.MX 6Sololite evaluation kit.

6

android_O8.0.0_1.0.0_image_6sxsabresd.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 6SoloX

7


android_O8.0.0_1.0.0_image_6sxsabreauto.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX

8

android_O8.0.0_1.0.0_image_7dsabresd.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 7Dual

9

fsl_aacp_dec_O8.0.0_1.0.0.tar.gz

AAC Plus Codec for O8.0.0_1.0.0

10

android_O8.0.0_1.0.0_tools.tar.gz

Manufacturing Toolkit and VivanteVTK for O8.0.0_1.0.0

 

  • Supported Hardware SoC/Boards:
    • i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform
    • i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform
    • i.MX 6SoloLite EVK platform
    • i.MX 6SoloX SABRE-SD board and platforms
    • i.MX 6SoloX SABRE-AI board and platforms
    • i.MX 7Dual SABRE-SD board and platform

 

  • Changes:

Compared to the N7.1.2_2.0.0 release, this release has the following major changes:

  • Upgraded the Android code base from android-7.1.2_r9 to android-8.0.0_r25.
  • Removed the device partition and added the vendor partition.
  • Enabled ION-based gralloc and EGL.
  • Feature:

For features please consult the release notes.

 

  • Known issues

For known issues and more details please consult the Release Notes.

标记 (2)
评论

hi,

 i git the source code base on the     source ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh  , but it use the googlesouce.com. it had the error: fatal:uable to access "https://android.googlesource/com/platform/external/bart/": Failed to connet to android.googlesource.com port 443:Connection timed out.

I am in China ,so Can you reply a way that  use  the  mirrors.tuna.tsinghua .edu.cn

pastedImage_1.png

为什么使用WIN10系统打开mfg tool烧写工具,在imx6q板子进入下载模式的时候,会有上图的提示。但是如果使用WIN7系统,则不会出现这个错误。之前android7.1.2的mfgtool烧写工具也出现这种情况。我使用的板子没有问题,android4.4.2\android5.1.1\anroid6.0.1\android7.1.1这几个系统在win10下烧写也是没有问题的。。

麻烦相关人员能帮忙查看一下!

you can use below features of git utility:

git config --global url.https://aosp.tuna.tsinghua.edu.cn.insteadOf https://android.googlesource.com

this will be replace url in git fetch request.

wilson chen 你好,i.mx6 的 android8.0的系统搭建,你搞定了吗?我这边在搭建环境是也遇到了相同的问题,如下:

fatal: unable to access 'https://android.googlesource.com/platform/external/neven/': Failed to connect to android.googlesource.com port 443: Connection refused
fatal: unable to access 'https://android.googlesource.com/platform/pdk/': Failed to connect to android.googlesource.com port 443: Connection refused
fatal: unable to access 'https://android.googlesource.com/platform/developers/demos/': Failed to connect to android.googlesource.com port 443: Connection refused
烦请指教下,谢谢!

I have same issue.   

你需要翻墙.

zarelaky‌ 也给了个墙内方法.你可以参照他去做.

之前已经解决,谢谢!

我repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-android-pie -m imx-p9.0.0_2.0.0-ga.xml后显示repo has been initialized in /home/sz/android_build

开始repo sync 显示fatal: unable to access 'https://source.codeaurora.org/external/imx/imx-manifest/': Failed to connect to localhost port 50321: Connection refused

fatal: unable to access 'https://android.googlesource.com/platform/external/libcxx/': Failed to connect to android.googlesource.com port 443: Connection refused
fatal: unable to access 'https://android.googlesource.com/platform/external/kernel-headers/': Failed to connect to android.googlesource.com port 443: Connection refused

请问如何解决,急急急

运行repo sync后完整输出信息是这样的:fatal: unable to access 'https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder/': GnuTLS recv error (-9): A TLS packet with unexpected length was received.
error: Cannot fetch platform/packages/apps/SoundRecorder from https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder
Fetching project platform/external/junit-params
fatal: unable to access 'https://android.googlesource.com/platform/external/sonivox/': Failed to connect to android.googlesource.com port 443: Connection refused

请问如何解决,我已经使用Aosp | 镜像站使用帮助 | 清华大学开源软件镜像站 | Tsinghua Open Source Mirror 替代了repo里的glooel

codeaurora use mirrors below:

git --config --global url." <mirror>".insteadOf "https://source.codeaurora.org"

<mirror> can be any one of below:

https://beijing.source.codeaurora.org

https://shanghai.source.codeaurora.org

if manifest.xml use "git://source.codeaurora.org" you must be edit

~/.gitconfig

add line below:

[url "https://beijing.source.codeaurora.org"]

insteadOf = git://codeaurora.org

你好,我执行Android_User's_Guide文件里的 make 2>&1 | tee build-log.txt 命令后显示:

device/fsl/imx8m/evk_8mm/AndroidBoard.mk:10: error: vendor/nxp/fsl-proprietary/media-profile/media-profile.mk: No such file or directory

请问是什么情况?如何解决,谢谢

无评分
版本历史
最后更新:
‎03-02-2018 12:53 AM
更新人: