WebGPU Vulkan Support on i.MX8MP (QtWebEngine 6.7.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WebGPU Vulkan Support on i.MX8MP (QtWebEngine 6.7.0)

1,160 Views
Aaronchou
Contributor I

Installing QtWebEngine 6.7.0 on imx8mp-lpddr4-evk
Chromium in QtWebEngine has started supporting WebGPU.
However, when I try the following flags:
--enable-unsafe-webgpu --enable-vulkan --use-angle=vulkan,
QtWebEngine crashes.

Is it because the BSP Vulkan support is not yet fully implemented?

Tags (1)
0 Kudos
Reply
4 Replies

598 Views
Aaronchou
Contributor I

 

Hi @Manuel_Salas 

I upgraded my system to BSP 6.12.3-lts and attempted to enable WebGPU and Vulkan.

The startup flags I used:

--enable-features=Vulkan,UseSkiaRenderer,WebGPUDeveloperFeatures --enable-unsafe-webgpu --ignore-gpu-blocklist --in-process-gpu --use-gl=egl

My Vulkan ICD config file (/etc/vulkan/icd.d/imx_icd.json):

{ "file_format_version": "1.0.0", "ICD": { "library_path": "/usr/lib/libvulkan_VSI.so.1", "api_version": "1.3.204" } }

Qt WebEngine does not crash, but the screen remains white with no rendering output.

When running vulkaninfo, I received the following warning:

WARNING: [Loader Message] Code 0 : loader_scanned_icd_add: Driver /usr/lib/libvulkan_VSI.so.1 supports Vulkan 1.3, but only supports loader interface version 2. Interface version 5 or newer required to support this version of Vulkan (Policy #LDP_DRIVER_7)

Please confirm whether the current Vulkan driver supports WebGPU functionality, or if an updated driver with loader interface version 5 or newer is required.

0 Kudos
Reply

1,135 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Aaronchou 

 

I hope you are doing very well.

As you can see on table 7 of RN00210 (Release Notes for LF6.6.52_2.2.0), Vulkan GPU is supported on the i.MX8MP:

Alejandro_Salas_0-1736875971039.png

 

I am not sure what BSP you are using, please check the respective release notes for your BSP.

Also, you can try:

--enable-unsafe-webgpu --enable-features=Vulkan

 

Best regards,

Salas.

 

0 Kudos
Reply

169 Views
Aaronchou
Contributor I

I have updated the BSP to BSP 6.12.3-lts.
WebGPU still doesn’t work.
I’ve posted my observations in the comments.
Is there any update?

0 Kudos
Reply

960 Views
vix
Contributor III

Hi @Manuel_Salas 

even with the flags you suggested, chromium is not able to see Vulkan and it reports

Vulkan: Disabled

 

Can you double check, please?

0 Kudos
Reply