[PATCH] Weston: g2d-renderer: Support weston-direct-display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[PATCH] Weston: g2d-renderer: Support weston-direct-display

2,032 Views
dothanhtrung
Contributor II

Hi,

I would like to propose a patch to support weston-direct-display in g2d-renderer.

My test environment is:

  • Board: Apalis i.MX8QM
  • Weston: lf-5.10.y-1.0.0

Weston config:

 

 

[core]
use-g2d=1
idle-time=0

 

 

In terminal, run test command:

 

 

weston-simple-dmabuf-egl -g

 

 

"-g" option to enable weston-direct-display

Expected result:

The weston demo app is displayed on screen.

Actual result:

Weston crashed.

 

After apply the patch, "weston-simple-dmabuf-egl -g" can run and display normally.

 

Edit: This patch also requires patch in https://community.nxp.com/t5/i-MX-Graphics/PATCH-Weston-cannot-propose-mixed-mode-state/td-p/1513894

0 Kudos
Reply
2 Replies

2,026 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Which kernel version is this?

You might contact Apalis.

Regards

0 Kudos
Reply

2,013 Views
dothanhtrung
Contributor II
Sorry. This patch is for weston-imx:
https://source.codeaurora.org/external/imx/weston-imx

> You might contact Apalis.
Okay. I will send the patch to them.

Thank you
0 Kudos
Reply