IMX8MM The weston service cannot be started after upgrading the yocto version.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM The weston service cannot be started after upgrading the yocto version.

1,555件の閲覧回数
Logan_Halo
Contributor I

U-Boot SPL 2022.04 (Jun 28 2024 - 10:48:10 +0800)
power_bd71837_init
DDRINFO: start DRAM init
DDRINFO: DRAM rate 2400MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.6(release):
NOTICE: BL31: Built : 05:32:10, Jun 27 2024


U-Boot 2022.04 (Jun 28 2024 - 10:48:10 +0800)

CPU: i.MX8MMQ rev1.0 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 33C
Reset cause: POR
Model: NXP i.MX8MM DDR4 EVK with CYW43455 WIFI/BT board
DRAM: 2 GiB
Core: 76 devices, 25 uclasses, devicetree: separate
NAND: 0 MiB
MMC: FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (1080 x 1920)
[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] rm67199_panel, panel
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated

BuildInfo:
- ATF

switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net:
Error: ethernet@30be0000 address not set.

Error: ethernet@30be0000 address not set.
No ethernet found.

Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
starting USB...
Bus usb@32e40000: USB EHCI 1.00
scanning bus usb@32e40000 for devices... 2 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
46537 bytes read in 2 ms (22.2 MiB/s)
Scanning disk mmc@30b50000.blk...
Found 3 disks
No EFI system partition

Error: ethernet@30be0000 address not set.

Error: ethernet@30be0000 address not set.
BootOrder not defined
EFI boot manager: Cannot load any image
MMC Device 2 not found
no mmc device at slot 2
Running BSP bootcmd ...
switch to partitions #0, OK
mmc1 is current device
Failed to load 'boot.scr'
31076864 bytes read in 331 ms (89.5 MiB/s)
Booting from mmc ...
46537 bytes read in 2 ms (22.2 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300e5c8

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.15.71+g50912be38601 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Tue Sep 12 22:17:59 UTC 2023
[ 0.000000] Machine model: FSL i.MX8MM DDR4 EVK with CYW43455 WIFI/BT board
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000098000000, size 640 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x97bc2800-0x97bc4fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s41368 r8192 d32360 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1370268K/2097152K available (18560K kernel code, 1548K rwdata, 7168K rodata, 2944K init, 543K bss, 71524K reserved, 655360K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000000] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.000383] Console: colour dummy device 80x25
[ 0.000446] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.000458] pid_max: default: 32768 minimum: 301
[ 0.000513] LSM: Security Framework initializing
[ 0.000600] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.000616] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.001954] rcu: Hierarchical SRCU implementation.
[ 0.002890] EFI services will not be available.
[ 0.003077] smp: Bringing up secondary CPUs ...
[ 0.003474] Detected VIPT I-cache on CPU1
[ 0.003504] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.003545] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.004033] Detected VIPT I-cache on CPU2
[ 0.004055] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.004081] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.004479] Detected VIPT I-cache on CPU3
[ 0.004499] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.004522] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.004581] smp: Brought up 1 node, 4 CPUs
[ 0.004607] SMP: Total of 4 processors activated.
[ 0.004613] CPU features: detected: 32-bit EL0 Support
[ 0.004618] CPU features: detected: 32-bit EL1 Support
[ 0.004624] CPU features: detected: CRC32 instructions
[ 0.012741] CPU: All CPU(s) started at EL2
[ 0.012776] alternatives: patching kernel code
[ 0.013950] devtmpfs: initialized
[ 0.020080] KASLR disabled due to lack of seed
[ 0.020225] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.020244] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.037191] pinctrl core: initialized pinctrl subsystem
[ 0.037699] DMI not present or invalid.
[ 0.038254] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.042999] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.043375] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.043727] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.043792] audit: initializing netlink subsys (disabled)
[ 0.043998] audit: type=2000 audit(0.040:1): state=initialized audit_enabled=0 res=1
[ 0.044549] thermal_sys: Registered thermal governor 'step_wise'
[ 0.044554] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.044734] cpuidle: using governor menu
[ 0.044919] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.045004] ASID allocator initialised with 65536 entries
[ 0.045870] Serial: AMBA PL011 UART driver
[ 0.045931] imx mu driver is registered.
[ 0.045950] imx rpmsg driver is registered.
[ 0.056395] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.065120] platform 32e10000.mipi_dsi: Fixing up cyclic dependency with 32e00000.lcdif
[ 0.065775] platform 32e30000.mipi_csi: Fixing up cyclic dependency with 32e20000.csi1_bridge
[ 0.086722] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.086741] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.086749] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.086756] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.087904] cryptd: max_cpu_qlen set to 1000
[ 0.090948] ACPI: Interpreter disabled.
[ 0.091622] iommu: Default domain type: Translated
[ 0.091630] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.091785] vgaarb: loaded
[ 0.092044] SCSI subsystem initialized
[ 0.092369] usbcore: registered new interface driver usbfs
[ 0.092408] usbcore: registered new interface driver hub
[ 0.092439] usbcore: registered new device driver usb
[ 0.093316] mc: Linux media interface: v0.10
[ 0.093343] videodev: Linux video capture interface: v2.00
[ 0.093407] pps_core: LinuxPPS API ver. 1 registered
[ 0.093414] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.093431] PTP clock support registered
[ 0.093589] EDAC MC: Ver: 3.0.0
[ 0.094627] FPGA manager framework
[ 0.094704] Advanced Linux Sound Architecture Driver Initialized.
[ 0.095196] Bluetooth: Core ver 2.22
[ 0.095223] NET: Registered PF_BLUETOOTH protocol family
[ 0.095229] Bluetooth: HCI device and connection manager initialized
[ 0.095238] Bluetooth: HCI socket layer initialized
[ 0.095246] Bluetooth: L2CAP socket layer initialized
[ 0.095263] Bluetooth: SCO socket layer initialized
[ 0.095851] clocksource: Switched to clocksource arch_sys_counter
[ 0.095996] VFS: Disk quotas dquot_6.6.0
[ 0.096036] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.096186] pnp: PnP ACPI: disabled
[ 0.101881] NET: Registered PF_INET protocol family
[ 0.102026] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.102948] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.102984] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.102997] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.103137] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.103349] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.103430] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.103475] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.103610] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.103996] RPC: Registered named UNIX socket transport module.
[ 0.104005] RPC: Registered udp transport module.
[ 0.104009] RPC: Registered tcp transport module.
[ 0.104015] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.104705] PCI: CLS 0 bytes, default 64
[ 0.105231] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.105891] kvm [1]: IPA Size Limit: 40 bits
[ 0.107100] kvm [1]: GICv3: no GICV resource entry
[ 0.107107] kvm [1]: disabling GICv2 emulation
[ 0.107121] kvm [1]: GIC system register CPU interface enabled
[ 0.107203] kvm [1]: vgic interrupt IRQ9
[ 0.107311] kvm [1]: Hyp mode initialized successfully
[ 0.110521] Initialise system trusted keyrings
[ 0.110656] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.116132] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.116695] NFS: Registering the id_resolver key type
[ 0.116729] Key type id_resolver registered
[ 0.116736] Key type id_legacy registered
[ 0.116810] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.116818] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.116842] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.117159] 9p: Installing v9fs 9p2000 file system support
[ 0.153074] Key type asymmetric registered
[ 0.153084] Asymmetric key parser 'x509' registered
[ 0.153136] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.153143] io scheduler mq-deadline registered
[ 0.153150] io scheduler kyber registered
[ 0.159550] EINJ: ACPI disabled.
[ 0.169922] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.169943] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.176041] mxs-dma 33000000.dma-controller: initialized
[ 0.177559] SoC: i.MX8MM revision 1.0
[ 0.178088] Bus freq driver module loaded
[ 0.183717] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.186008] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 47, base_baud = 5000000) is a IMX
[ 0.186521] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 48, base_baud = 5000000) is a IMX
[ 0.186920] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 49, base_baud = 1500000) is a IMX
[ 1.218449] printk: console [ttymxc1] enabled
[ 1.238361] loop: module loaded
[ 1.242730] of_reserved_mem_lookup() returned NULL
[ 1.247598] megasas: 07.717.02.00-rc1
[ 1.252900] imx ahci driver is registered.
[ 1.325477] nand: device found, Manufacturer ID: 0xf0, Chip ID: 0xf0
[ 1.331861] nand: Unknown gpmi-nand
[ 1.335348] nand: bus width 8 instead of 16 bits
[ 1.339972] nand: No NAND device found
[ 1.343753] gpmi-nand: probe of 33002000.nand-controller failed with error -22
[ 1.355079] tun: Universal TUN/TAP device driver, 1.6
[ 1.360964] thunder_xcv, ver 1.0
[ 1.364243] thunder_bgx, ver 1.0
[ 1.367499] nicpf, ver 1.0
[ 1.372280] hclge is initializing
[ 1.375611] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.382840] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.388203] e1000: Intel(R) PRO/1000 Network Driver
[ 1.393087] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.398872] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.403841] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.409849] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.415255] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.420862] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.427134] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.433239] sky2: driver version 1.30
[ 1.437489] usbcore: registered new interface driver r8152
[ 1.443228] VFIO - User Level meta-driver version: 0.3
[ 1.450601] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.457151] ehci-pci: EHCI PCI platform driver
[ 1.461638] ehci-platform: EHCI generic platform driver
[ 1.467068] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.473271] ohci-pci: OHCI PCI platform driver
[ 1.477755] ohci-platform: OHCI generic platform driver
[ 1.483702] usbcore: registered new interface driver uas
[ 1.489074] usbcore: registered new interface driver usb-storage
[ 1.495150] usbcore: registered new interface driver usbserial_generic
[ 1.501698] usbserial: USB Serial support registered for generic
[ 1.507733] usbcore: registered new interface driver ftdi_sio
[ 1.513500] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.520839] usbcore: registered new interface driver usb_serial_simple
[ 1.527386] usbserial: USB Serial support registered for carelink
[ 1.533500] usbserial: USB Serial support registered for zio
[ 1.539178] usbserial: USB Serial support registered for funsoft
[ 1.545202] usbserial: USB Serial support registered for flashloader
[ 1.551578] usbserial: USB Serial support registered for google
[ 1.557517] usbserial: USB Serial support registered for libtransistor
[ 1.564064] usbserial: USB Serial support registered for vivopay
[ 1.570089] usbserial: USB Serial support registered for moto_modem
[ 1.576374] usbserial: USB Serial support registered for motorola_tetra
[ 1.583007] usbserial: USB Serial support registered for nokia
[ 1.588860] usbserial: USB Serial support registered for novatel_gps
[ 1.595235] usbserial: USB Serial support registered for hp4x
[ 1.601000] usbserial: USB Serial support registered for suunto
[ 1.606938] usbserial: USB Serial support registered for siemens_mpi
[ 1.613328] usbcore: registered new interface driver usb_ehset_test
[ 1.622458] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.637056] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.643272] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.652437] i2c_dev: i2c /dev entries driver
[ 1.657683] mx6s-csi 32e20000.csi1_bridge: initialising
[ 1.666562] Bluetooth: HCI UART driver ver 2.3
[ 1.671030] Bluetooth: HCI UART protocol H4 registered
[ 1.676180] Bluetooth: HCI UART protocol BCSP registered
[ 1.681514] Bluetooth: HCI UART protocol LL registered
[ 1.686659] Bluetooth: HCI UART protocol ATH3K registered
[ 1.692081] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.698441] Bluetooth: HCI UART protocol Broadcom registered
[ 1.704121] Bluetooth: HCI UART protocol QCA registered
[ 1.710863] sdhci: Secure Digital Host Controller Interface driver
[ 1.717067] sdhci: Copyright(c) Pierre Ossman
[ 1.722106] Synopsys Designware Multimedia Card Interface Driver
[ 1.728744] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.736466] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.743375] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.750303] usbcore: registered new interface driver usbhid
[ 1.755889] usbhid: USB HID core driver
[ 1.764211] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.773181] galcore: clk_get vg clock failed, disable vg!
[ 1.778883] Galcore version 6.4.3.p4.398061
[ 1.841675] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 0
[ 1.851023] hantrodec 0 : module inserted. Major = 510
[ 1.856696] hantrodec 1 : module inserted. Major = 510
[ 1.862622] hx280enc: module inserted. Major <509>
[ 1.873063] NET: Registered PF_LLC protocol family
[ 1.878325] NET: Registered PF_INET6 protocol family
[ 1.885227] Segment Routing with IPv6
[ 1.888944] In-situ OAM (IOAM) with IPv6
[ 1.892912] NET: Registered PF_PACKET protocol family
[ 1.898988] Bluetooth: RFCOMM TTY layer initialized
[ 1.903885] Bluetooth: RFCOMM socket layer initialized
[ 1.909063] Bluetooth: RFCOMM ver 1.11
[ 1.912827] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.918145] Bluetooth: BNEP filters: protocol multicast
[ 1.923381] Bluetooth: BNEP socket layer initialized
[ 1.928353] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.934280] Bluetooth: HIDP socket layer initialized
[ 1.939968] 8021q: 802.1Q VLAN Support v1.8
[ 1.944177] lib80211: common routines for IEEE802.11 drivers
[ 1.949951] 9pnet: Installing 9P2000 support
[ 1.954259] tsn generic netlink module v1 init...
[ 1.959038] Key type dns_resolver registered
[ 1.964202] Loading compiled-in X.509 certificates
[ 1.992559] usb_phy_generic usbphynop1: supply vcc not found, using dummy regulator
[ 2.000335] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[ 2.008670] usb_phy_generic usbphynop2: supply vcc not found, using dummy regulator
[ 2.016408] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[ 2.071756] LDO6: supplied by regulator-dummy
[ 2.077152] i2c i2c-0: IMX I2C adapter registered
[ 2.083041] i2c 1-003d: Fixing up cyclic dependency with 32e10000.mipi_dsi
[ 2.090281] adv7511 1-003d: supply avdd not found, using dummy regulator
[ 2.097087] adv7511 1-003d: supply dvdd not found, using dummy regulator
[ 2.103829] adv7511 1-003d: supply pvdd not found, using dummy regulator
[ 2.110571] adv7511 1-003d: supply a2vdd not found, using dummy regulator
[ 2.117398] adv7511 1-003d: supply v3p3 not found, using dummy regulator
[ 2.124141] adv7511 1-003d: supply v1p2 not found, using dummy regulator
[ 2.132565] adv7511 1-003d: Probe failed. Remote port 'mipi_dsi@32e10000' disabled
[ 2.140408] i2c 1-0050: Fixing up cyclic dependency with 32e40000.usb
[ 2.148228] i2c i2c-1: IMX I2C adapter registered
[ 2.154450] pca953x 2-0020: using no AI
[ 2.158971] pca953x 2-0020: failed writing register
[ 2.165022] i2c 2-003c: Fixing up cyclic dependency with 32e30000.mipi_csi
[ 2.172334] ov5640_mipi 2-003c: No sensor reset pin available
[ 2.178128] ov5640_mipi 2-003c: supply DOVDD not found, using dummy regulator
[ 2.185363] ov5640_mipi 2-003c: supply DVDD not found, using dummy regulator
[ 2.192457] ov5640_mipi 2-003c: supply AVDD not found, using dummy regulator
[ 2.208863] ov5640_mipi 2-003c: Read reg error: reg=300a
[ 2.214189] ov5640_mipi 2-003c: Camera is not found
[ 2.219331] i2c i2c-2: IMX I2C adapter registered
[ 2.226492] imx6q-pcie 33800000.pcie: supply epdev_on not found, using dummy regulator
[ 2.228518] imx-drm 32c00000.bus:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 2.234759] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.243321] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 2.255754] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e10000 to encoder DSI-34: -19
[ 2.267351] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[ 2.275625] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -19
[ 2.276216] imx6q-pcie 33800000.pcie: PCIe PLL is locked.
[ 2.283293] imx-drm 32c00000.bus:display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[ 2.288740] imx6q-pcie 33800000.pcie: iATU unroll: enabled
[ 2.298315] [drm] Initialized imx-drm 1.0.0 20120507 for 32c00000.bus:display-subsystem on minor 1
[ 2.303137] imx6q-pcie 33800000.pcie: Detected iATU regions: 4 outbound, 4 inbound
[ 2.303150] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[ 2.317407] pps pps0: new PPS source ptp0
[ 2.319697] imx6q-pcie 33800000.pcie: IO 0x001ff80000..0x001ff8ffff -> 0x0000000000
[ 2.339165] imx6q-pcie 33800000.pcie: MEM 0x0018000000..0x001fefffff -> 0x0018000000
[ 2.347485] imx6q-pcie 33800000.pcie: iATU unroll: enabled
[ 2.353033] imx6q-pcie 33800000.pcie: Detected iATU regions: 4 outbound, 4 inbound
[ 2.363650] fec 30be0000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 2.370493] fec 30be0000.ethernet: Using random MAC address: ee:dd:a9:af:ca:f0
[ 2.381392] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.393463] mxc_mipi-csi 32e30000.mipi_csi: supply mipi-phy not found, using dummy regulator
[ 2.402201] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered
[ 2.409178] CSI: Registered sensor subdevice: mxc_mipi-csi.0
[ 2.414860] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 333000000
[ 2.425189] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 2 mkt segment 2 supported-hw 0x4 0x4
[ 2.434696] Hot alarm is canceled. GPU3D clock will return to 64/64
[ 2.444881] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 2.445552] sdhci-esdhc-imx 30b40000.mmc: allocated mmc-pwrseq
[ 2.451045] input: bd718xx-pwrkey as /devices/platform/soc@0/30800000.bus/30a20000.i2c/i2c-0/0-004b/gpio-keys.1.auto/input/input1
[ 2.468723] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.479990] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.480286] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.487881] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 2.493693] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.503043] ALSA device list:
[ 2.509281] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.520094] No soundcards found.
[ 2.757523] mmc1: host does not support reading read-only switch, assuming write-enable
[ 2.799664] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 2.807665] mmcblk1: mmc1:aaaa SK32G 29.7 GiB
[ 2.814628] mmcblk1: p1 p2
[ 3.369025] imx6q-pcie 33800000.pcie: Phy link never came up
[ 3.374752] imx6q-pcie: probe of 33800000.pcie failed with error -110
[ 3.419279] EXT4-fs (mmcblk1p2): recovery complete
[ 3.425799] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null). Quota mode: none.
[ 3.435681] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.443078] devtmpfs: mounted
[ 3.446762] Freeing unused kernel memory: 2944K
[ 3.451366] Run /sbin/init as init process
[ 3.645271] systemd[1]: System time before build time, advancing clock.
[ 3.669484] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 3.701161] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 5.15-kirkstone (kirkstone)!

[ 3.772900] systemd[1]: Hostname set to <imx8mm-ddr4-evk>.
[ 3.831214] systemd-sysv-generator[187]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.855598] systemd-sysv-generator[187]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.880227] systemd-sysv-generator[187]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.904564] systemd-sysv-generator[187]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.928618] systemd-sysv-generator[187]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.953602] systemd-sysv-generator[187]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.978062] systemd-sysv-generator[187]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.002092] systemd-sysv-generator[187]: SysV service '/etc/init.d/rc.local' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.298088] systemd[1]: Queued start job for default target Graphical Interface.
[ 4.348477] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 4.374443] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 4.398439] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 4.422121] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 4.444268] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 4.468189] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 4.492198] systemd[1]: Reached target Host and Network Name Lookups.
[ OK ] Reached target Host and Network Name Lookups.
[ 4.516063] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 4.535998] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 4.555971] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 4.576712] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 4.601458] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 4.624744] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 4.644837] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 4.664924] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 4.689147] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 4.713043] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.736764] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.757066] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.781881] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.804512] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.816811] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 4.844612] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 4.868169] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.895930] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.916377] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[ 4.933341] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 4.957898] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes...
[ 4.984164] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 5.007707] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 5.031706] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 5.045147] fuse: init (API version 7.34)
[ 5.056406] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 5.072190] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[ 5.085147] systemd[1]: systemd-journald.service: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 5.098094] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 5.110855] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.132305] systemd[1]: Load Kernel Modules was skipped because all trigger condition checks failed.
[ 5.145328] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network …ts from Kernel command line...
[ 5.171588] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 5.186488] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null). Quota mode: none.
[ 5.200028] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 5.223622] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 5.249723] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 5.272843] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
[ OK ] Finished Apply Kernel Variables.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 5.549779] systemd-journald[199]: Received client request to flush runtime journal.
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /var/volatile...
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Mounted /var/volatile.
[ OK ] Finished Coldplug All udev Devices.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Finished Create Volatile Files and Directories.
[ OK ] Started Rule-based Manager for Device Events and Files.
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
Starting Weston socket...
Starting Console System Startup Logging...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Listening on Weston socket.
[ OK ] Finished Console System Startup Logging.
[ OK ] Reached target Socket Units.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ 6.482824] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 24
[ 6.489149] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 25
[ 6.495341] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 26
[ 6.501864] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 27
[ OK ] Started Periodic Command Scheduler Registered IR keymap rc-empty
[0m.
[ 6.535495] rc rc0: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0
[ 6.544045] input: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0/input2
Starting D-Bus System Message Bus...
[ 6.577282] random: dbus-daemon: uninitialized urandom read (12 bytes read)
[ 6.592626] debugfs: File 'Playback' in directory 'dapm' already present!
[ 6.599503] debugfs: File 'Capture' in directory 'dapm' already present!
[ OK ] Started Linux Firmware Loader Daemon.
[ 6.629694] random: dbus-daemon: uninitialized urandom read (12 bytes read)
[ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S).
[ 6.657879] imx-sdma 30bd0000.dma-controller: firmware found.
[ 6.657878] imx-sdma 302b0000.dma-controller: firmware found.
[ 6.657982] imx-sdma 302b0000.dma-controller: loaded firmware 4.6
[ 6.677075] imx-sdma 302c0000.dma-controller: firmware found.
Starting IPv6 Packet Filtering Framework...
[ 6.741337] caam 30900000.crypto: device ID = 0x0a16040100000000 (Era 9)
[ 6.748717] caam 30900000.crypto: job rings = 2, qi = 0
Starting IPv4 Packet Filtering Framework...
[ 6.806354] caam-snvs 30370000.caam-snvs: ipid matched - 0x3e
[ 6.812388] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state
Starting Network Time Service (one-shot ntpdate mode)...
Starting Telephony service...
[ OK ] Started System Logging Service.
Starting User Login Management...
[ OK ] Started TEE Supplicant.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Finished Network Time Service (one-shot ntpdate mode).
[ OK ] Started Telephony service.
[ OK ] Reached target Preparation for Network.
[ OK ] Reached target Hardware activated USB gadget.
Starting Connection service...
Starting Network Configuration...
[ OK ] Started User Login Management.
[ OK ] Started Connection service.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Network Configuration.
[ OK ] Reached target Network.
Starting containerd container runtime...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started Respond to IPv6 Node Information Queries.
Starting /etc/rc.local Compatibility...
[ OK ] Started Network Router Discovery Daemon.
Starting Permit User Sessions...
[ OK ] Finished Load/Save Random Seed.
[ OK ] Started /etc/rc.local Compatibility.
[ 7.763376] caam algorithms registered in /proc/crypto

[ 7.777233] caam 30900000.crypto: caam pkc algorithms registered in /proc/crypto
[ 7.787254] caam 30900000.crypto: rng crypto API alg registered prng-caam
[ 7.803940] caam 30900000.crypto: registering rng-caam
[ OK ] Started 7.816304] Device caam-keygen registered
;39mAvahi mDNS/DNS-SD Stack.
Starting Save/Restore Sound Card State...
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttymxc1.
[ OK ] Reached target Login Prompts.
Starting Hostname Service...
Starting Weston, a Wayland…ositor, as a system service...
Starting WPA supplicant...
[ OK ] Finished Save/Restore Sound Card State.
[ OK ] Reached target Sound Card.
Starting User Database Manager...
[ OK ] Started WPA supplicant.
[ OK ] Started Hostname Service.
[ OK ] Started User Database Manager.
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Found device /dev/mmcblk1p1.
[ OK ] Created slice User Slice of UID 0.
Starting File System Check on /dev/mmcblk1p1...
Starting User Runtime Directory /run/user/0...
[ OK ] Finished User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ 8.528486] audit: type=1006 audit(1651172664.748:2): pid=491 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ 8.540858] audit: type=1300 audit(1651172664.748:2): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffdd1279b0 a2=1 a3=ffffa8423020 items=0 ppid=1 pid=491 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[ 8.567224] audit: type=1327 audit(1651172664.748:2): proctitle="(systemd)"
[ OK ] Finished File System Check on /dev/mmcblk1p1.
Mounting /run/media/boot-mmcblk1p1...
[ OK ] Mounted /run/media/boot-mmcblk1p1.
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of User root.
[ 8.916628] audit: type=1006 audit(1651172665.136:3): pid=468 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses=4294967295 ses=2 res=1
[ 8.929075] audit: type=1300 audit(1651172665.136:3): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffdd1279b0 a2=1 a3=ffffa8423020 items=0 ppid=1 pid=468 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
[ 8.955180] audit: type=1327 audit(1651172665.136:3): proctitle="(weston)"
[ OK ] Started containerd container runtime.
[ OK ] Reached target Multi-User System.
[FAILED] Failed to start Weston, a …mpositor, as a system service.
See 'systemctl status weston.service' for details.
[ OK ] Reached target Graphical Interface.
Starting Record Runlevel Change in UTMP...
[ OK ] Finished Record Runlevel Change in UTMP.

NXP i.MX Release Distro 5.15-kirkstone imx8mm-ddr4-evk ttymxc1

0 件の賞賛
返信
2 返答(返信)

1,527件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

it need to build again please download the latest yocto bsp and compile.

Regards

0 件の賞賛
返信

1,507件の閲覧回数
Logan_Halo
Contributor I
Hello,
I have also tried using imx-6.6.3-1.0.0.xml and encountered the same problem.
The version I used before was imx-5.4.47-2.2.0.xml.
0 件の賞賛
返信