IMX8 GPU crash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8 GPU crash

642 次查看
JoRadio
Contributor I

When I run the Benchmark test of Qt5.15 on IMX8, the system crashed after running for half an hour, and the GPU printed the dump information. What causes this? The Texture Size I use is 1024x1024. I enable IBL Lighting and SkyBox. The Material used is Original Material, and the default values are selected for other configurations.

This is the download link for Benchmark:

BenchmarkDemo · master · public-demos / qtquick3d · GitLab

The attachment is the print information after the GPU crash.

 

0 项奖励
回复
2 回复数

390 次查看
amy598cross
Contributor I

Hello @JoRadio,
The crash is likely due to GPU memory exhaustion. The i.MX8MP’s Vivante GC7000UL GPU has limited memory, and enabling IBL Lighting, SkyBox, and using 1024×1024 textures can overwhelm it over time. Try reducing texture size to 512×512 or disabling IBL/SkyBox incrementally to isolate the cause.

Best Regards,
Amy Cross


0 项奖励
回复

559 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi @JoRadio 

Sorry to reply late, Which BSP code do you use? 

The i.MX8MP uses the Vivante GC7000UL GPU, which has limited GPU memory.
Enabling Image-Based Lighting (IBL) and SkyBox with large textures (1024x1024) can consume significant GPU memory.

Here are some suggestions:

1. Reduce texture resolution:

Reduce the texture from 1024x1024 to 512x512 or 256x256 and observe if it still crashes.


2. Gradual disabling feature:

First, turn off the SkyBox or IBL lighting and gradually identify which feature is causing the problem.

B.R

 

0 项奖励
回复