I.MX8 LCD display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8 LCD display

504 Views
SeedsHIRO
Contributor I

Does I.mx8PLUS have the ability to flip the LCD display upside down?

0 Kudos
Reply
1 Reply

479 Views
joanxie
NXP TechSupport
NXP TechSupport

i.mx8ulp has PXP which can support this feature, refer to the reference manual:

The PXP module includes following features:

Scaling

Supports YUV 422, 420, 444 and any RGB formatted pixels

The maximum downscaling factor can be up to 16

Color Space Conversion (CSC)

Supports converting from YUV to RGB

Supports bypass mode

Supports color space coefficients configuration

Secondary Color Space Conversion (CSC2)

Supports converting to RGB or YUV color spaces depending on the desired output pixel format

Supports color space coefficients configuration


Rotation

Supports 0, 90, 180, 270 degrees

Supports vertical and horizontal flips

Composite Alpha Blending and Color Key

Supports normal alpha blending and Porter-Duff alpha blending.

Supports color key function to create transparent effects on the output pixel

0 Kudos
Reply