I.MX8 LCD display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX8 LCD display

1,212件の閲覧回数
SeedsHIRO
Contributor I

Does I.mx8PLUS have the ability to flip the LCD display upside down?

0 件の賞賛
返信
1 返信

1,187件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

i.mx8ulp has PXP which can support this feature, refer to the reference manual:

The PXP module includes following features:
•
Scaling
—
Supports YUV 422, 420, 444 and any RGB formatted pixels
—
The maximum downscaling factor can be up to 16
•
Color Space Conversion (CSC)
—
Supports converting from YUV to RGB
—
Supports bypass mode
—
Supports color space coefficients configuration
•
Secondary Color Space Conversion (CSC2)
—
Supports converting to RGB or YUV color spaces depending on the desired output pixel format
—
Supports color space coefficients configuration

•
Rotation
—
Supports 0, 90, 180, 270 degrees
—
Supports vertical and horizontal flips
•
Composite Alpha Blending and Color Key
—
Supports normal alpha blending and Porter-Duff alpha blending.
—
Supports color key function to create transparent effects on the output pixel

0 件の賞賛
返信