HDMI, LVDS two screen logo display problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI, LVDS two screen logo display problems

1,736 Views
chen-wust
Contributor II

dear all

Phenomenon:The main screen is lvds interface, resolution is 1980*1080. The secondary screen is HDMI interface, resolution is 1280*1024. When the kernel displays the logo, both screens are displayed by obtaining data from /dev/fb0. Because the resolution is different, the display of the logo always has a screen display position that is wrong.

       I was wondering if there was a way to turn off the HDMI display. Or the two screens use different fb. At present, fb is virtual out of fb_helper in drm framework. I hope to get your help.

 

0 Kudos
Reply
1 Reply

1,523 Views
Letu
Contributor I

Hello, I had the same problem. Have you solved this problem? Thanks.

0 Kudos
Reply