Gui Guider

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gui Guider

Jump to solution
5,290 Views
K314X
Contributor II

Hi,

I am using a MIMXRT1064-EVK board with a rk043fn02h Rocketch display. I saw the new Gui Guider tool and wanted to give it a go but I am not able to run anything. Only the PrinterDemo displays something on the board but the touch seems to not be working. I tried to create a project from scratch or use another demo but nothing would be displayed on the screen. But there are no compilation or flashing error I can see. 

Any idea why it would display something for one demo and nothing for the others ?

Thanks for the help 

0 Kudos
Reply
1 Solution
5,266 Views
K314X
Contributor II

Hi, the issue seems to have been that the second ribbon of the display was not properly connected (the touch controller ?). I unplugged the display and put it back again and now it works.

I am new to NXP dev boards but are display often to be put on the other side of the boards with none of the gpio/sensors/buttons ? Or is it only for the MiMXRT1064 ?

But so it was my bad in the end... Thanks

View solution in original post

0 Kudos
Reply
3 Replies
5,276 Views
OmarBengoa
Contributor II

Hi, I use MiMXRT1050 board and all run ok, touch too. Did you select the correct board on creating project?

0 Kudos
Reply
5,267 Views
K314X
Contributor II

Hi, the issue seems to have been that the second ribbon of the display was not properly connected (the touch controller ?). I unplugged the display and put it back again and now it works.

I am new to NXP dev boards but are display often to be put on the other side of the boards with none of the gpio/sensors/buttons ? Or is it only for the MiMXRT1064 ?

But so it was my bad in the end... Thanks

0 Kudos
Reply
5,249 Views
OmarBengoa
Contributor II

In my board MiMXRT1050 the display put on the side without buttons, leds, connectors, etc. that is strage but that's the way it is. 

0 Kudos
Reply