Gralloc and HWcomposer explanation and DRM buffer sharing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gralloc and HWcomposer explanation and DRM buffer sharing

3,201件の閲覧回数
dkenjic
Contributor I

Greetings to NXP support teams,

 

I would like to confirm and understand two things in regards with your Android graphics workflow for i.mx8qm board

One clarification in advance, all materials I would refer to are from NXP official releases and github

- https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/android-os-for-i-m...

- https://github.com/nxp-imx-android

1) Gralloc and HWcomposer 

As far as I understood, gralloc.imx uses gralloc_viv.imx for acessing DRM modules. After flashing your Android demo image (Android Q10.0.0_2.6.0 in particular), I can see both of them loaded and utilized. On the other hand, I can see only hwcomposer.imx loaded and utilized, although hwcomposer_viv.imx prebuilt can also be found within materials provided by NXP.

What is the use of hwcomposer_viv.imx and is it actually needed in order to have Android graphics fully leveraging GPU?

2) DRM Buffer sharing

In order to enable buffer sharing DRM principles, Gralloc and HWcomposer must share handle for particular graphics buffer. Is this handle provided by your Memory structure inheriting the native_handle or there is some more proprietary code used for this purpose which is not available as open source. 

 

Best regards,

Dusan

0 件の賞賛
返信
1 返信

3,154件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

FYI.

More information about GPU and DPU in Chapter 5 and 6 in this document.

https://www.nxp.com.cn/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

0 件の賞賛
返信