GPU accelerated image flipping on imx8mq

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPU accelerated image flipping on imx8mq

1,342 次查看
szilard_b_cib
Contributor II

Dear NXP Team,

I need to use the GPU to flip my image for low latency with the i.MX 8M Quad (i.MX8MQ) processor. I discovered that the i.MX8MQ does not support 2D graphics, which excludes the use of imxcompositor_g2d and imxvideoconvert_g2d, so I need to use OpenGL for this task. The pipeline in [1] works well on my PC; however, on GStreamer [2] (Mickledore Yocto), the same pipeline displays the video without flipping it. When I replace glvideoflip method=horizontal-flip with gltransformation scale-x=-1, the video flips but freezes immediately [3]. Although I managed to use the rotate method in glimagesink to flip the entire video, this approach isn't feasible since I am displaying multiple camera streams in a mosaic and can't use a sink for each one. I attached the output of the pipeline [3]

Do you have any suggestions for resolving this issue?

Best regards,
Szilard B


[1] gst-launch-1.0 filesrc location="/media/szibes/szilard/test_screen.mp4" ! qtdemux name=demux \
demux.video_0 ! queue ! h264parse ! avdec_h264 ! videoconvert ! glupload ! glvideoflip method=horizontal-flip ! glimagesink sync=false enable-last-sample=false qos=false force-aspect-ratio=false render-rectangle='<0, 0,1920,1080>'

[2] gst-inspect-1.0 version 1.22.0
GStreamer 1.22.0
Unknown package origin

[3] gst-launch-1.0 filesrc location="/path/to/test_video.mp4" ! qtdemux name=demux \
demux.video_0 ! queue ! h264parse ! vpudec ! videoconvert ! glupload ! gltransformation scale-x=-1 ! glimagesink

标记 (3)
0 项奖励
回复
2 回复数

1,317 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Correct the iMX8M does not support OpenVG and it does not support video flipping, you have made a workaround but you code freeze since glupload is searching for the 2d on GPU, this is a bug in out system, and will report it, but unfortunately we don;t have a workaround.

Regards

0 项奖励
回复

1,307 次查看
szilard_b_cib
Contributor II

Hello,

I noticed that the glimagesink can flip the image on the GPU. Would it be possible for the NXP GStreamer developers to add an option to gltransformation to use affine transformations when the G2D library is not available, similar to how glimagesink handles flipping?

Best regards,
Szilard B

0 项奖励
回复