コミュニティを検索
03-29-2016
02:40 PM
EUF-DES-T1741 - Scalable Multicore QorIQ Layerscape Processors Based on 64-bit Software Environment for Enterprise, Home and Industrial Applications
09-09-2019
06:56 AM
LX2160A is NXP’s highest performance multicore device with 16 Arm-v8 64-bit A72 cores at up to 2.2 GHz. It also has 24 SerDes lanes running at 25 GHz supporting dual 100GE interfaces and up to 24 lan...
- タグ:
- lx2160a
12-05-2016
11:08 AM
03-13-2017
02:11 PM
The Layerscape LS1028A industrial applications processor includes a TSN-enabled Ethernet switch and Ethernet controllers to support converged IT and OT networks. Two powerful 64-bit ARM v8 cores s...
ラベル:
10-31-2018
12:35 PM
Do you plan to secure your data transmission keeping high data throughput, low-power and CPU load? The Layerscape family is your best choice.
06-10-2019
05:31 PM
...ill review the use of NXP’s multicore processors in traditional safety critical applications, and the retroactive analysis of the Layerscape product family’s fault detection mechanisms and coverage.
- タグ:
- layerscape
04-27-2022
04:30 PM
Is there any GUI based configuration tool for mapping pin peripherals on a layerscape processor (such as the LS1012A)? I don't see support for this in MCUXpresso, nor have I found any dedicated c...
- タグ:
- ls1012a
05-04-2015
05:04 AM
...echnologies such as EtherCAT, PROFINET and EtherNet/IP are testament to this. In this session, we will explore how QorIQ LS1 processor families can help equipment manufacturers span this landscape using a...
03-29-2016
03:07 PM
EUF-NET-T1745 - An overview of ARMv8 virtualization technology, its integration in NXP Layerscape ARMv8-based SoC's and its enablement through the QorIQ SDK .
10-25-2021
02:20 AM
...nderlying network infrastructure. This document describes DPDK basic introduction, DPDK core components, DPDK Linux networking, DPDK Crypto Subsystem, DPDK memory manager and DPDK implementation on Layerscape...