コミュニティを検索
Hi NXP team, Hello, I would like to ask, can the PCA943X connected to a coil directly obtain energy from the phone's NFC, or is another chip needed? Thank you!
返信の結果を表示(8)
-
Hello Tomas, This means I don't need to purchase any NFC chips, right? If I still need a little b...
-
...rom you for a long time. I hope you are well.I am not using NFC for communication, only for power s...
-
Hello Fabian Thank you very much for your response. Here is my requirement: I need an NFC chip t...
-
Hello ZHELI1 , NTAG5 can provide up to 30mW. But do you need any NFC communication or o...
-
...atched, I aligned the mobile phone NFC with the coil, and then connected the output to a small LED l...
-
Hello Tomas, I haven't heard from you for a long time. I hope you are well.I am not using NFC f...
-
...ncluding an MCU + NFC Tag. For your application, the NTAG5 (Link or Switch) might be used. The NTAG5 has a...
-
Hello ZHELI1, You have to tuned the NFC antenna using CP and CS to approx 13.56...
12-11-2024
12:40 PM
Hello everyone, this post is intended to add support to one of the most popular NFC chips on the market (PN532).
On this example I will use the I.MX93 EVK as reference board and focused in I...
03-17-2026
04:31 AM
...ntenna, except for the NFC reader components itself.
During development of new readers, this calibration shall be done each time the antenna design, antenna matching, or EMC filter is modified....
4 週間前
1件の賞賛
Introduction.
This document provides a guide on how to use the NFC frontend PN5190 with the FRDM-MCXN947 and using the latest existing version of the NFC Reader Library.
The hardware r...
ラベル:
10-19-2017
12:55 AM
3件の賞賛
Introduction I am trying to make one page that contain all the useful information about NFC Antenna Design. I will keep update and add the information to this page when I found something useful. &n...
09-17-2025
07:06 AM
...alibrate LPCD
Run "Endless I/Q read"
Check how the I and Q values change
With no card/object in the antenna proximity
with a NFC card/object in the antenna proximity
T...
12-10-2020
01:36 AM
6件の賞賛
You are a salesperson or FAE and are looking for ways to sell more Near-Field-Communication (NFC) products? This community provides ideas, information, and materials that help you to s...
11-19-2024
12:26 AM
Hi all, I have a small query which requires your help. PN532 provide: I2C,SPI,UART as host interface. I am looking for an alternate for PN532. consideration point: 1. UART host interfa...
ラベル
04-28-2025
11:05 PM
1件の賞賛
This article describes how to evaluate ULPCD feature together with PN7642 EVK (OM27642EVK) and NFC Cockpit.
1// Disable DC-DC in EEPROM
OM27642EVK does not required any HW changes f...
10-31-2016
12:49 AM