コミュニティを検索
1ヶ月前
Hi, Regarding the functional safety of i.MX95, I noticed that there is a safety manual available, but it requires an NDA. Could I know what content is in this document? How do I sign an NDA? A...
1ヶ月前
With my 'regular' (i.e. without having signed any kind of NDA or similar arrangements) NXP account, I can access the Safety Peripheral driver for the K3 and K5 family. But it seems for the K1 f...
2 週間前
I need to enable the SM1.INTERCONNECT_EDC_GASKET safety mechanism for my project. I am using AUTOSAR RTD 3.0.0 and the S32 Design Studio (S32DS) tool to generate the code. Could you please c...
07-01-2026
09:37 AM
1. Does the Safety Peripheral Drivers *replace* the real time driver or augments it? 2. Are both of these (or one or none) are provided in source form? 3. Is there any per-unit royalty when t...
06-14-2018
02:58 PM
Functional safety awareness level one. Introduction to functional safety, what it is, why and how it is implemented. This overview session provides the building blocks for the other deep dive t...
08-03-2026
07:26 AM
...nteractions and expected outcomes. Release Note : specifies that following release has limitations Information requested: Precise safety goal(s) and ECC scheme assumed Which SRAM i...
06-03-2026
04:05 AM
HI. 1.我想使用MC33774的SME6功能安全机制完成断线诊断。但是当我回读SECM_SYNC_VB0~VB17时,我获取到的寄存器值大部分都是0x8001,其他的通道都是负压,只有我把我的电池电芯全部调整到3.8V以上时能够回读正常得到电压值,一旦某个单体电压稍低,我就只能读到大部分都是0x8001。(我和这个参考步骤中唯一的不同是我的延时等待时间为100ms)。这是为什么?这个诊断机...
11-07-2025
01:38 AM
1. Is the MCAL package for S32K148 ASIL-compliant, and does it include a safety case and safety manual to demonstrate compliance for a specific ASIL level? 2. If we have the document S...
返信の結果を表示(3)
-
Hello, From your explanation, does the S32K1_RTD_4.4_Safety_Manual completely cover the safety...
-
...he safety aspects of the MCAL modules included within RTD, or is there also a separate MCAL-specific Safety...
-
...ncludes the S32K148. This compliance is supported by: Safety Manual Failure Modes Effects and D...
2 週間前
2件の賞賛
...ultiple software functions onto a single, powerful processor. This consolidation reduces cost, weight, and complexity, but it introduces a critical challenge: how do you run a safety-critical AUTOSAR b...
01-18-2026
08:24 PM
Hi , We are working on an ASIL B project using the S32M244 chip. Currently, our project IDE is S32DS, but it seems that it has not yet obtained functional safety...
返信の結果を表示(3)
-
Hello, S32DS is just development studio/ eclipse based. The issue is gcc compiler which is not safety...
-
Hello, For S32M244 functional‑safety development, Keil MDK cannot currently be used, because no K...
-
...bout it, as below: 已解决: Re: Feasibility of Developing S32K3 ASIL B Functional Safety Products U...