コミュニティを検索
12-02-2025
02:39 PM
Porting an ST Application
This section outlines the process of migrating an application developed in the STM32Cube IDE to the NXP MCUXpresso IDE, using a compatible SDK for the target N...
12-30-2025
11:50 AM
Clone an Example Project from MCUXpresso IDE
The following steps will guide you through the manipulation of the general-purpose outputs. The example sets up a CTimer to generate a PWM signal and c...
07-01-2025
02:02 AM
We are pleased to announce that MCUXpresso IDE v25.06 (build 136) is now available.
This is a maintenance release that builds upon the previous MCUXpresso IDE v24.12 release and we r...
12-30-2025
10:20 AM
The most recent versions of MCUXpresso IDE count with a terminal emulation application. This tool can be used to display information sent from your NXP development platform's virtual serial port
1....
07-30-2026
12:35 AM
3件の賞賛
Hi everyone, Is MCUXpresso IDE still supported? In the last years there was a MCUXpresso IDE upgrade every about 4 months. Since june 2025 there is not upgrades. Does this mean t...
01-15-2025
03:34 AM
We are pleased to announce that MCUXpresso IDE v24.12 (build 148) is now available.
This is a maintenance release that builds upon the previous MCUXpresso IDE v24.09 release a...
10-02-2024
02:18 PM
1件の賞賛
We are pleased to announce that MCUXpresso IDE v24.9 (build 25) is now available.
This is a maintenance release that builds upon the previous MCUXpresso IDE v11.10.0 release a...
07-05-2024
05:38 AM
We are pleased to announce that MCUXpresso IDE v11.10.0 (build 3148) is now available.
This is a maintenance release that builds upon the previous MCUXpresso IDE v11.9.1 release a...
12-30-2025
11:26 AM
The following steps will guide you through the hello_world demo application using MCUXpresso IDE for the Cortex-M33 application. The MCUXpresso IDE installation and the SDK for the MCXN-Series can b...
02-23-2026
01:12 AM
In the MCUXpresso IDE, the config tools updates are disabled by default. To update Config Tools integrated in the MCUXpresso IDE follow these steps:
Select Manage..., check MCUXpresso Config T...