MCUXpresso IDE roadmap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE roadmap

Jump to solution
852 Views
biafra
Senior Contributor I

Hi everyone,

 

Is MCUXpresso IDE still supported?

 

In the last years there was a MCUXpresso IDE upgrade every about 4 months. Since june 2025 there is not upgrades. Does this mean that MCUXpresso IDE will not be upgraded in the future?

 

Many thanks

Biafra

1 Solution
823 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @biafra ,

Thanks for your post.

At present, there are no plans for a new MCUXpresso IDE roadmap. Our primary focus and recommended development environment is MCUXpresso for Visual Studio Code | NXP Semiconductors.

However, the latest MCUXpresso IDE v25.06 is still actively maintained, and you can continue to import and use SDKs for new devices without any issues.

Please note that if you use the integrated Config Tools for newer products, make sure to update the Config Tools package manually. For detailed instructions, please refer to: Updating Config Tools in the MCUXpresso IDE - NXP Community.

Hope it helps.

BR

Celeste

View solution in original post

5 Replies
824 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @biafra ,

Thanks for your post.

At present, there are no plans for a new MCUXpresso IDE roadmap. Our primary focus and recommended development environment is MCUXpresso for Visual Studio Code | NXP Semiconductors.

However, the latest MCUXpresso IDE v25.06 is still actively maintained, and you can continue to import and use SDKs for new devices without any issues.

Please note that if you use the integrated Config Tools for newer products, make sure to update the Config Tools package manually. For detailed instructions, please refer to: Updating Config Tools in the MCUXpresso IDE - NXP Community.

Hope it helps.

BR

Celeste

577 Views
danielkrol
Contributor III
Thank you for the clarification.

Since MCUXpresso IDE v25.06 is still actively maintained, could you please confirm whether NXP plans to fix the known macOS issue with selecting multiple lines of code in the editor?

The underlying Eclipse/SWT issue appears to have already been identified and fixed upstream. If NXP plans to include this fix in MCUXpresso IDE, could you please let us know when we can expect it to be available?

Best regards,
Daniel
0 Kudos
Reply
546 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @danielkrol ,

Sorry, I checked with the internal team and learned that there is currently no confirmed update plan. You can click Receive alerts on the product page to receive notifications about any possible future updates

Free Professional ARM Development Tools | NXP Semiconductors

Celeste_Liu_0-1788432533469.png

 

BR

Celeste

0 Kudos
Reply
590 Views
Microsystemca
Contributor II

How do we create a new project in the VSC MCUXpresso extension if the device/board is not listed in the library? It seems like if the part number SDK is not in the list, we can't create the project...... (The create project button is greyed out.)

 

0 Kudos
Reply
583 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @Microsystemca , could you please create a new post on MCUXpresso for VSCode - NXP Community

0 Kudos
Reply