コミュニティを検索
01-19-2024
03:25 AM
6件の賞賛
..._difResolution_add_HPD.diff which supports HPD feature.
Notion: pleas add force-on=true to the output you use as main screen. For example.
EXTENDED display and higher BSP update
s...
05-28-2025
01:32 PM
1件の賞賛
This document provides a step-by-step guide to building the NXP Auto Linux Yocto BSP using WSL 2 (Windows Subsystem for Linux) instead of a full virtual machine or native Linux i...
ラベル:
06-18-2020
07:59 AM
Best practices for vulnerability monitoring and remediation
10-24-2014
05:32 PM
01-16-2022
09:54 PM
2件の賞賛
This doc explain our Linux BSP driver and how to custom them. Contests as follows: include bsp30/32
目录 1 S32G Linux文档说明 ................................................. 2 2 创建S32G RDB2 Linux板级开发...
ラベル:
05-15-2014
01:52 PM
Clone Wizard does launch on my Win7 64-bit PC for any version of MQX4.0 or 4.1. I get the following error: Here is he version of Java I am running:
05-28-2025
02:36 AM
...xample below:
Prepare the working scripts/patches mentioned in the previous link mentioned: git clone https://github.com/nxp-auto-linux/linux-bsp-utils.git
cd linux-bsp-utils/codeaurora_migration/
M...
ラベル:
04-24-2013
07:18 AM
...ake the BSP for the official hardware, I use the BSPCloningWizard tool to clone the twrk60d100m BSP that I think is the closest BSP for my project. I successfully compile the twrk60d100m clone (bsp, p...
08-28-2014
05:21 AM
1件の賞賛
I am currently testing KDS + MQX. MQX comes with KDS ready libraries for many evaluation boards. But the cloning wizard is missing the KDS IDE target, making difficult to port it on my own p...
01-30-2025
09:37 AM
1件の賞賛
...ernel setup and navigate into it:
$ mkdir FRDM-IMX93-Kernel
$ cd FRDM-IMX93-Kernel
4. Cloning the Kernel patches
Retrieve the necessary kernel patches from the NXP repository:
$ git clone...