コミュニティを検索
08-03-2026
12:15 AM
...mpossible to launch the application. Is there a way to re-authenticate the changed FBL using the HMAC Key, thereby allowing both the FBL and the application to run normally? When running the H...
05-20-2026
09:23 AM
...bsp;Root of Trust Key Hash (RoTKTH) and SB3KDK Encryption key as well as hoe to active debug authentication before to move Lifecycle states.
ラベル:
05-19-2025
12:14 PM
From APDU manual 4.6.2 DisableObjectCreation command: This command can only be used in a session that used the credential with identifier RESERVED_ID_RESTRICT as authentication object. 0...
- タグ:
- se05x
ラベル
- ラベル:
-
SecId
返信の結果を表示(6)
-
Hi @Kan_Li - I have now found the answer in the APDU guide: 3.2.3 Authentication o...
-
Hi @psvz , Yes, I agree Symmetric authentication model requires authent...
-
Hi @Kan_Li The authentication object is provisioned as Key-Id: 0X7fff0200 A...
-
...oesn't take symmetric key provisioned in SE under that ID. Symmetric authentication model requires authent...
-
...ou please confirm with the manufacturer the max length of AES key for authentication SE05X s...
-
...onfirm 256-bits length is supported for authentication?
09-02-2026
02:39 AM
...eturned was KEY_EMPTY. Additionally, within Fota_S32k3_SecureBootProcess, the hseRequestResult value is also returned as KEY_EMPTY, causing retVal to be 1 (NOT_OK). Because this authentication fails, S...
11-18-2019
05:29 PM
Description
Biometric authentication devices use an MCU or MPU to perform biometrics with the integration of peripherals such as a PC or a wireless connectivity module to communicate w...
ラベル:
10-09-2023
08:25 PM
1件の賞賛
...olution
Additional Information
Customers authenticating additional software images from a bootloader not provided by an NXP BSP, should ensure correct authentication is being p...
06-14-2018
03:22 PM
Introduction to A100x secure authenticators including new A1007, as part of overall training authentication protocols, what to look for in security IC and potential use cases.
05-06-2019
04:40 PM
Introduction to A100x secure authenticator, authentication protocols, what to look for in security IC, and potential use cases.
- タグ:
- a100x
06-10-2025
08:12 AM
Hello NXP community, I am using SE051 with embedded Linux, where I store private key in SE051 and certificate is in file system, embedded Linux board run as TLS server and want to enable mutual authentication...
ラベル
- ラベル:
-
SE050
08-26-2022
09:20 AM
...hown although the communication between the accessManager and SE05X is secured here with PlatfSCP03 keys. 2. Among the three different authentication mechanisms available, Could you please e...
- タグ:
- se05x
ラベル
- ラベル:
-
SE050
返信の結果を表示(8)
-
...ifferent authentication mechanisms available, Could you please elaborate on what authentication m...
-
...mong the three different authentication mechanisms available, Could you please elaborate on what authentication...
-
Thanks @Kan_Li . In the authentication based sessions, I think the policies really m...
-
...or MW building would start the authentication process automatically when you run any ex_xxx e...
-
...eparate build environment. All session authentication mechanisms are supported, platform SCP03 must be o...
-
...uring the openssl engine building within the MW, so the specified authentication would start a...
-
...ant to enable user authentication based sessions in my application using openssl, I would first use&n...
-
...uthID? How? - Yes, it is possible. Just as I mentioned in https://community.nxp.com/t5/Secure-Authentication...