Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
3,828 results
Sorted by:
05-23-2025
08:45 AM
2 Kudos
...nstall the MCUXpresso IDE, or use the MCUXpresso Installer for VS Code to install the necessary software tools.
Download Firmware
Get the latest firmware from the Segger w...
03-29-2022
09:03 AM
...onditions have not yet been fully met, i.e. have not been true and false.
With Ozone and J-Trace PRO, code coverage analysis is completely non-intrusive. It does not require modified code or a...
04-30-2014
05:52 AM
2 Kudos
NOTE: the screenshots below are for KDS V1.0.1-beta! After creating a new debug configuration is simple: Select either 'GDB OpenOCD Debugging', 'GDB PEMicro Interface Debugging' or 'GDB SEGGER...
Labels:
Show results in comments (3)
-
...nd I was scratching my head regarding what to do with my j-link (segger). Lifesaver once again Erich!
-
...he KW40 is not supported. I have not used it for the KW40 and used P&E and Segger instead. I can l...
-
...t basically means the GDB client cannot connect to the OpenOCD server (see the same message for Segger...
04-18-2023
08:09 PM
4 Kudos
...ollowing error will appear.
Modified the "Debug configurations" for S32 Design Studio platform V3.4
Change the highlighted part to the path below.
C:\Program Files (x86)\SEGGER...
01-21-2026
01:16 AM
Hi, I want to read and write eFuses of a RT1165 on a custom board. I am using the J-Trace Pro and flashing in IDE works fine, but the Secure Provisioning Tool (SEC) v25.12 is not able to connec...
- Tags:
- efuse
03-26-2017
08:48 PM
4 Kudos
On OSX by using the same FRDM-K22F board and Onboard OpenSDA/J-Link, with KDS 3.2 I can debug w/o problem, but with MCUXpresso 10 I can't. It seems MCUX doesn't provide proper commands to arm-none-ea...
Labels
- Labels:
-
General
Show results in replies (7)
-
...ave this: C:\nxp\KDS_3.2.0\eclipse\../segger/JLinkGDBServerCL -if swd -device MK64FN1M0xxx12 -e...
-
Hi Nirvana, have you downloaded and installed as well the latest SEGGER J-Link software from SEGGER...
-
Hi Nirvana, ah, sorry, I have missed that. One thing to note or check: using the SEGGER f...
-
...ther thing in the log is that I see you are using quite an old version of the SEGGER OpenSDA f...
-
...CUXpresso IDE User Guide (chapter 9, as well as the SEGGER specific information in sections 3.8 -&g...
-
Here's the log: Executing Server: /Applications/SEGGER/JLink/JLinkGDBServer -nosilent -s...
-
...nexpected OK from the SEGGER gdb server... 195,232 13^error,msg="Unknown remote qXfer reply: OK" w...
02-21-2022
09:25 AM
Hi, I am trying to use the new Segger RTT communication plugin. Of course I am running the latest freemaster target driver with net transport and segger_rtt. This is my freemaster_cfg.h: &n...
Show results in replies (5)
-
...eems to be no issue with FreeMASTER desktop app, using SEGGER RTT communication channel in passive mode....
-
...nyway I think I am loosing interest for this SEGGER RTT connectivity option. Do I read correctly h...
-
...MSTR_NET // Use network transport layer #define FMSTR_NET_DRV FMSTR_NET_SEGGER_RTT // Use network driver for SEGGER...
-
...9021 SEGGER J-Link V7.56d - Real time terminal output J-Link OpenSDA compiled May 27 2019 10:59:5...
-
Dear Luca, thanks for making the experiment. The error code says there was a timeout when waiting...
05-08-2026
01:58 AM
Hello! We have been experimenting with WCT-15W1 board; this is equipped with Freescale 56800EX MCU (WCT1013). We don't have a compatible programmer (P&E), only Segger JLink devices. Is t...
01-31-2024
02:55 PM
Hello! I am having a problem creating a new GDB SEGGER Interface Debugging configuration. Whenever I try to create a new one I get prompted with the message: The launch configuration 'p...
Show results in replies (4)
-
...o a simple led_blinky test, wrote the development board download firmware as SEGGER Jlink, and c...
-
...aunch configuration dialog of Eclipse. If you do it there, make sure you create it under 'GDB SEGGER I...
-
...ollowing: This happens just after double clicking the GDB SEGGER Interface Debugging option on the left p...
-
...sing Segger's ozone for debugging instead which works every time without a hitch.
08-07-2014
02:37 AM
1 Kudo
This document explains how you can debug the FRDM-K22F board with the Segger J-Link OpenSDAv2.1 Firmware and the Kinetis Design Studio V1.1.0. Applicable to: OpenSDAv2.1 boards (FRDM-K...
Labels: