tflite Failed to apply NNAPI delegate. on imx8qmmek BSP 5.4.24-2.1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tflite Failed to apply NNAPI delegate. on imx8qmmek BSP 5.4.24-2.1.0

2,441件の閲覧回数
korabelnikov
Contributor III

I use python to load and run my tflite model converted from tensorlfow(keras) resnet18 model

interpreter = tflite.Interpreter(model_path=model_name)

 It works with float32 model and prints out 

INFO: Created TensorFlow Lite delegate for NNAPI.
Applied NNAPI delegate.
561.8170 ms ± 0.1711 ms (std)

 

but when I use uint8 quantized model I've got

INFO: Created TensorFlow Lite delegate for NNAPI.
Failed to apply NNAPI delegate.
275.3198 ms ± 0.1635 ms (std)

 

I have another resnet18 model converted to tflite earlier. It works with NNApi and takes 34 ms.

 

My question is How should I convert models from tensorflow to make nnapi works in tflite on imx8.

 

ラベル(1)
1 返信

2,159件の閲覧回数
yochaytzur
Contributor I

Did you solve that? I'm having the same problem.

 

0 件の賞賛