eIQ support for Tensorflow in Linux 5.4.24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eIQ support for Tensorflow in Linux 5.4.24

ソリューションへジャンプ
3,639件の閲覧回数
Paul_Kang
NXP Employee
NXP Employee

Hello,

I tried to run Tensorflow example which is described in 6.1. Running benchmark application and 8.1.2. TensorFlow tests of eIQ user manual UM11226, but I found that they are not working and they require library installed by tensorflow.

In our previous BSP, 4.14.98, which was base of UM11226, we can build Tensorflow together but it seems we can't in latest 5.4.24 BSP version. 

Could you let me know if we can build Tensorflow in 5.4.24 version? 

If it is dropped, could you let us know the reason and our suggestion for it? 

I tested above with i.MX8M Mini EVK board. 

Best regards,

Paul

ラベル(1)
0 件の賞賛
1 解決策
3,590件の閲覧回数
manish_bajaj
NXP Employee
NXP Employee

paulkang‌,

Please check latest Linux release document.  UM11226 is applicable with 4.14.98. eIQ is now part of Yocto release.

Current road map is to support Tensorflow Lite, ARMNN, ONNX and OpenCV( only on CPU).

You can try building Tensorflow with latest 5.4.24 though we have not done any test from our side.

-Manish 

元の投稿で解決策を見る

0 件の賞賛
1 返信
3,591件の閲覧回数
manish_bajaj
NXP Employee
NXP Employee

paulkang‌,

Please check latest Linux release document.  UM11226 is applicable with 4.14.98. eIQ is now part of Yocto release.

Current road map is to support Tensorflow Lite, ARMNN, ONNX and OpenCV( only on CPU).

You can try building Tensorflow with latest 5.4.24 though we have not done any test from our side.

-Manish 

0 件の賞賛