eIQ support for Tensorflow in Linux 5.4.24

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eIQ support for Tensorflow in Linux 5.4.24

跳至解决方案
3,766 次查看
Paul_Kang
NXP Employee
NXP Employee

Hello,

I tried to run Tensorflow example which is described in 6.1. Running benchmark application and 8.1.2. TensorFlow tests of eIQ user manual UM11226, but I found that they are not working and they require library installed by tensorflow.

In our previous BSP, 4.14.98, which was base of UM11226, we can build Tensorflow together but it seems we can't in latest 5.4.24 BSP version. 

Could you let me know if we can build Tensorflow in 5.4.24 version? 

If it is dropped, could you let us know the reason and our suggestion for it? 

I tested above with i.MX8M Mini EVK board. 

Best regards,

Paul

标签 (1)
0 项奖励
1 解答
3,717 次查看
manish_bajaj
NXP Employee
NXP Employee

paulkang‌,

Please check latest Linux release document.  UM11226 is applicable with 4.14.98. eIQ is now part of Yocto release.

Current road map is to support Tensorflow Lite, ARMNN, ONNX and OpenCV( only on CPU).

You can try building Tensorflow with latest 5.4.24 though we have not done any test from our side.

-Manish 

在原帖中查看解决方案

0 项奖励
1 回复
3,718 次查看
manish_bajaj
NXP Employee
NXP Employee

paulkang‌,

Please check latest Linux release document.  UM11226 is applicable with 4.14.98. eIQ is now part of Yocto release.

Current road map is to support Tensorflow Lite, ARMNN, ONNX and OpenCV( only on CPU).

You can try building Tensorflow with latest 5.4.24 though we have not done any test from our side.

-Manish 

0 项奖励