eIQ Toolkit Ubuntu Installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eIQ Toolkit Ubuntu Installation

ソリューションへジャンプ
10,621件の閲覧回数
AlanWen
Contributor IV

I installed the eIQ Toolkit v1.8.0 within Ubuntu 20.04 as below command:

1. Download eIQ Toolkit Installer from https://www.nxp.com/design/software/eiq-ml-development-environment/eiq-toolkit-for-end-to-end-model-...

2. unzip eiq-toolkit-v1.8.0.40-1_am64_b230711.deb.zip

3. chmod a+x eiq-toolkit-v1.8.0.40-1_am64_b230711.deb.bin

4. ./eiq-toolkit-v1.8.0.40-1_am64_b230711.deb.bin

After installed the eiq-toolkit v1.8.0 I had found the icon in my ubuntu apps but there is nothing happened after I clicking the eiq-toolkit icon. And there is no way for me to open the toolkit from terminal.

Is there any way I can do to install the eiq-toolkit in ubuntu 20.04 ?

ラベル(1)
タグ(3)
0 件の賞賛
1 解決策
10,599件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi, 

  eIQ is installed into the /opt/nxp/eIQ_Toolkit_v1.8.0 folder on Linux. You should be able to open it from the command by running: 

/opt/nxp/eIQ_Toolkit_v1.8.0/bin/eiqqenv.sh

/opt/nxp/eIQ_Toolkit_v1.8.0/eiq-portal

 

-Anthony

元の投稿で解決策を見る

1 返信
10,600件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi, 

  eIQ is installed into the /opt/nxp/eIQ_Toolkit_v1.8.0 folder on Linux. You should be able to open it from the command by running: 

/opt/nxp/eIQ_Toolkit_v1.8.0/bin/eiqqenv.sh

/opt/nxp/eIQ_Toolkit_v1.8.0/eiq-portal

 

-Anthony