eIQ Toolkit Ubuntu Installation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eIQ Toolkit Ubuntu Installation

跳至解决方案
10,470 次查看
AlanWen
Contributor IV

I installed the eIQ Toolkit v1.8.0 within Ubuntu 20.04 as below command:

1. Download eIQ Toolkit Installer from https://www.nxp.com/design/software/eiq-ml-development-environment/eiq-toolkit-for-end-to-end-model-...

2. unzip eiq-toolkit-v1.8.0.40-1_am64_b230711.deb.zip

3. chmod a+x eiq-toolkit-v1.8.0.40-1_am64_b230711.deb.bin

4. ./eiq-toolkit-v1.8.0.40-1_am64_b230711.deb.bin

After installed the eiq-toolkit v1.8.0 I had found the icon in my ubuntu apps but there is nothing happened after I clicking the eiq-toolkit icon. And there is no way for me to open the toolkit from terminal.

Is there any way I can do to install the eiq-toolkit in ubuntu 20.04 ?

标签 (1)
标记 (3)
0 项奖励
1 解答
10,448 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi, 

  eIQ is installed into the /opt/nxp/eIQ_Toolkit_v1.8.0 folder on Linux. You should be able to open it from the command by running: 

/opt/nxp/eIQ_Toolkit_v1.8.0/bin/eiqqenv.sh

/opt/nxp/eIQ_Toolkit_v1.8.0/eiq-portal

 

-Anthony

在原帖中查看解决方案

1 回复
10,449 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi, 

  eIQ is installed into the /opt/nxp/eIQ_Toolkit_v1.8.0 folder on Linux. You should be able to open it from the command by running: 

/opt/nxp/eIQ_Toolkit_v1.8.0/bin/eiqqenv.sh

/opt/nxp/eIQ_Toolkit_v1.8.0/eiq-portal

 

-Anthony