build eIQ image failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

build eIQ image failed

1,590 次查看
g0930421313
Contributor II

Hi

I'm building an eIQ image for my imx8mqevk and encountered an issue as following....
what should i do?

OS : Ubuntu16.04 in VMware 

ERROR: tensorflow-1.12.0-r0 do_configure: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)
ERROR: Logfile of failure stored in: /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900
Log data follows:
| DEBUG: Executing shell function do_configure
| downloading https://bitbucket.org/eigen/eigen/get/fd6845384b86.tar.gz
|
| gzip: stdin: unexpected end of file
| tar: Child returned status 1
| tar: Error is not recoverable: exiting now
| WARNING: exit code 2 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)
ERROR: Task (/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6041 tasks of which 0 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure
Summary: There were 14 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

0 项奖励
0 回复数