build eIQ image error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

build eIQ image error

1,824 次查看
g0930421313
Contributor II

Hi

I'm building an eIQ image for my imx8mqevk. I followed the User Manual "UM11226" step by step but encountered following error after execute the "bitbake fsl-image-qt5" at 3.2.6.
what should i do ?

OS : Ubuntu 16.04 in VMware Workstation 15 Player

 

NOTE: Your conf/bblayers.conf has been automatically updated.

Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:05:48

Parsing of 2577 .bb files complete (0 cached, 2577 parsed). 3499 targets, 221 skipped, 8 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

NOTE: Multiple providers are available for runtime ptpd (ptpd, ptpd-qoriq)

Consider defining a PREFERRED_RPROVIDER entry to match ptpd

NOTE: Multiple providers are available for runtime ptpd-dev (ptpd, ptpd-qoriq)

Consider defining a PREFERRED_RPROVIDER entry to match ptpd-dev

 

Build Configuration:

BB_VERSION           = "1.38.0"

BUILD_SYS            = "x86_64-linux"

NATIVELSBSTRING      = "ubuntu-16.04"

TARGET_SYS           = "aarch64-poky-linux"

MACHINE              = "imx8mqevk"

DISTRO               = "fsl-imx-xwayland"

DISTRO_VERSION       = "4.14-sumo"

TUNE_FEATURES        = "aarch64"

TARGET_FPU           = ""

meta                

meta-poky            = "HEAD:c9bd4984f8f471ca2c43052714f4413ba99cf171"

meta-oe             

meta-multimedia      = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"

meta-freescale       = "HEAD:27ca94f8a4336790ba117b4298566f6820e7e74c"

meta-freescale-3rdparty = "HEAD:82037216280a39957fb4272581637abec734ad50"

meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"

meta-bsp            

meta-sdk             = "HEAD:8eeb420fad668b733ab95b460895e1c337c66b25"

meta-browser         = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"

meta-gnome          

meta-networking     

meta-python         

meta-filesystems     = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"

meta-qt5             = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"

meta-imx-machinelearning = "HEAD:7e9294dead55d1f6b4f1cfe486e0c4e0c5097953"

 

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:19

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: nspr-native-4.19-r0 do_fetch: Failed to fetch URL http://ftp.mozilla.org/pub/nspr/releases/v4.19/src/nspr-4.19.tar.gz, attempting MIRRORS if available

WARNING: nss-native-3.35-r0 do_fetch: Failed to fetch URL http://ftp.mozilla.org/pub/mozilla.org/security/nss/releases/NSS_3_35_RTM/src/nss-3.35.tar.gz, attempting MIRRORS if available

WARNING: mesa-2_17.3.8-r0 do_fetch: Failed to fetch URL https://mesa.freedesktop.org/archive/mesa-17.3.8.tar.xz, attempting MIRRORS if available

WARNING: icu-native-60.2-r0 do_fetch: Checksum mismatch for local file /home/stu/fsl-arm-yocto-bsp/downloads/icu4c-60_2-src.tgz

Cleaning and trying again.

WARNING: icu-native-60.2-r0 do_fetch: Renaming /home/stu/fsl-arm-yocto-bsp/downloads/icu4c-60_2-src.tgz to /home/stu/fsl-arm-yocto-bsp/downloads/icu4c-60_2-src.tgz_bad-checksum_e869986174e1719338a3baf5b95ca4f2

WARNING: icu-native-60.2-r0 do_fetch: Checksum failure encountered with download of http://download.icu-project.org/files/icu4c/60.2/icu4c-60_2-src.tgz - will attempt other sources if available

WARNING: leptonica-1.74.4-r0 do_fetch: Checksum mismatch for local file /home/stu/fsl-arm-yocto-bsp/downloads/leptonica-1.74.4.tar.gz

Cleaning and trying again.

WARNING: leptonica-1.74.4-r0 do_fetch: Renaming /home/stu/fsl-arm-yocto-bsp/downloads/leptonica-1.74.4.tar.gz to /home/stu/fsl-arm-yocto-bsp/downloads/leptonica-1.74.4.tar.gz_bad-checksum_294113120dc2d94ae2f9555eea7f0bd0

WARNING: leptonica-1.74.4-r0 do_fetch: Checksum failure encountered with download of http://leptonica.com/source/leptonica-1.74.4.tar.gz - will attempt other sources if available

WARNING: opencv-4.0.1+gitAUTOINC+c9ad5779f2_2522124473_32e315a5b1_34e4206aef_fccf7cd6a4_d29d003e00-r0 do_configure: QA Issue: opencv: invalid PACKAGECONFIG: neon [invalid-packageconfig]

WARNING: libeigen-3.3.4-r0 do_fetch: Failed to fetch URL http://bitbucket.org/eigen/eigen/get/3.3.4.tar.bz2;downloadfilename=libeigen-3.3.4.tar.bz2, attempting MIRRORS if available

WARNING: nbench-byte-2.2.3-r0 do_fetch: Failed to fetch URL https://fossies.org/linux/misc/nbench-byte-2.2.3.tar.gz, attempting MIRRORS if available

WARNING: sudo-1.8.22-r0 do_fetch: Failed to fetch URL http://ftp.sudo.ws/sudo/dist/sudo-1.8.22.tar.gz, attempCurrently  2 running tasks (5388 of 8934)  60% |#####################################################WARNING: lttng-modules-2.10.6-r0 do_package: lttng-modules: no modules were created; this may be due to CONFIG_TRACEPOINTS not being enabled in your kernel.

ERROR: tensorflow-1.12.0-r0 do_configure: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)

ERROR: Logfile of failure stored in: /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900

Log data follows:

| DEBUG: Executing shell function do_configure

| downloading https://bitbucket.org/eigen/eigen/get/fd6845384b86.tar.gz

|

| gzip: stdin: unexpected end of file

| tar: Child returned status 1

| tar: Error is not recoverable: exiting now

| WARNING: exit code 2 from a shell command.

| ERROR: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)

ERROR: Task (/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure) failed with exit code '1'

NOTE: Tasks Summary: Attempted 6041 tasks of which 0 didn't need to be rerun and 1 failed.

 

Summary: 1 task failed:

  /home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure

Summary: There were 14 WARNING messages shown.

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

 

标签 (1)
0 项奖励
0 回复数