Using machine learning with a simple yocto project image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using machine learning with a simple yocto project image

1,919 Views
Olatz
Contributor I

I would like to know if it is possible to use machine learning software (my device is the i.MX 8 M mini). I want to know if i can do that building only the core-image-base Yocto Project image or an image more simple than the full one (the one recommended for ML). We have a console based device. 

Thank you.

0 Kudos
0 Replies