Keras and imx8m Plus GPU/ML module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Keras and imx8m Plus GPU/ML module

2,050 次查看
mpolo
Contributor I

Hi,

I'm working with the i.MX 8M Plus EVK to test the ML accelerator integrated in the SoC.

To do that, I've created a Keras model with TensorFlow 1.15. Now I would like to run it on the GPU/ML module of the i.MX 8M Plus.

The eIQ user's guide (rev. L5.4.24_2.1.0) says:
"The GPU/ML module driver does not support per-channel quantization yet. Therefore post-training quantization of models with TensorFlow v2 cannot be used if the model is supposed to run on the GPU/ML module (inference on CPU does not have this limitation). TensorFlow v1 quantization-aware training and model conversion is recommended in this case".

It seems that Keras quantization-aware training only supports TensorFlow v2 and it is per-channel/per-axis for convolutional layers: https://www.tensorflow.org/model_optimization/guide/quantization/training#general_support_matrix.

Is there a way to do per-tensor quantization for a Keras model with convolutional layers and run it on the GPU/ML module? If not, how am I supposed to run my model on the GPU/ML module?

标签 (1)
0 项奖励
0 回复数