Imx8mqevk GPU Applications.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8mqevk GPU Applications.

11,255 Views
manizillion
Contributor IV

Hi ,

CAn I use video based OpenCV applications to run on the imx8 GPU,

Do I need OpenCL for it ?

If so can you share OpenCV applications which video streaming based ..

Labels (1)
Tags (1)
0 Kudos
16 Replies

10,816 Views
manish_bajaj
NXP Employee
NXP Employee

[email protected]‌,

Can you elaborate when you say object detection application is very slow response on imx8mqevk?

What is slow? Inference speed is low or image capture is slow. What others feature are enabled in back ground?

-Manish

0 Kudos

10,806 Views
manizillion
Contributor IV

Hi Manish,

I am trying to inlcude meta-ml meta-sdk layers into agl linux build. I am using these layers from latest L5.4.24_2.1.0 release on imx8mqevk. But i do get error for armnn do_compile errors  . How to solve these merge issues ?

Can i merge these builds into other build environment?

ERROR: armnn-19.08-r1 do_compile: Execution of '/home/administrator/jellyfish5.4/build/tmp/work/aarch64-agl-linux/armnn/19.08-r1/temp/run.do_compile.19578' failed with exit code 127:
/home/administrator/jellyfish5.4/build/tmp/work/aarch64-agl-linux/armnn/19.08-r1/temp/run.do_compile.19578: 1: eval: cmake: not found
WARNING: exit code 127 from a shell command.

ERROR: Logfile of failure stored in: /home/administrator/jellyfish5.4/build/tmp/work/aarch64-agl-linux/armnn/19.08-r1/temp/log.do_compile.19578

0 Kudos

10,816 Views
manizillion
Contributor IV

Thanks Manish,

We were running a face detection algorithm with opencv using v4l2  mipi csi camera from nxp, Although the face detection is happening but response seen on the display is very slow. Application does not hang though.  Any issue with v4l and opencv compatability ? In background we have enabled the following in local.conf.

#Configure the OpenCV package:
IMAGE_INSTALL_append = "opencv python-opencv"

PACKAGECONFIG_remove_pn-opencv_mx8 = "python3"
PACKAGECONFIG_append_pn-opencv_mx8 = " dnn jasper openmp test neon python2 qt5 gtk "

#Add CMake for SDK’s cross-compile:

TOOLCHAIN_HOST_TASK_append += " nativesdk-cmake nativesdk-make"

IMAGE_INSTALL_append = " \
flatbuffers \
arm-compute-library \
tensorflow-lite \
armnn \
armnn-onnx \
stb \
"

PREFERRED_VERSION_opencv = "4.0.1%"

#Remove the OpenCL support from packages
PACKAGECONFIG_remove_pn-opencv_mx8 = "opencl"
PACKAGECONFIG_remove_pn-arm-compute-library = "opencl"

0 Kudos

10,816 Views
manish_bajaj
NXP Employee
NXP Employee

[email protected]‌,

 There can various reason because of that performance might not be optimal. What is the output of top? Share your application with us.

-Manish

0 Kudos

10,816 Views
manizillion
Contributor IV

Hi Manish,

Here is the app code below, how to make this piece of code run on gpu ? will it be faster if it runs on gpu?

// CPP program to detects face in a video

// Include required header files from OpenCV directory
#include "opencv2/objdetect.hpp"
#include "opencv2/highgui.hpp"
#include "opencv2/imgproc.hpp"
#include <iostream>

using namespace std;
using namespace cv;

// Function for Face Detection
void detectAndDraw( Mat& img, CascadeClassifier& cascade, CascadeClassifier& nestedCascade, double scale);
//void detectAndDisplay( Mat& frame, CascadeClassifier& fullbodycascade, CascadeClassifier& bodycascade);

int main( int argc, const char** argv )
{
// VideoCapture class for playing video for which faces to be detected
VideoCapture capture;
Mat frame, image;

// PreDefined trained XML classifiers with facial features
// CascadeClassifier upperbodycascade, fullbodycascade;
CascadeClassifier facecascade, eyecascade;
double scale=1;

// Load classifiers from "opencv/data/haarcascades" directory
//nestedCascade.load("haarcascade_eye_tree_eyeglasses.xml") ;

// Change path before execution
//fullbodycascade.load( "haarcascade_fullbody.xml" ) ;
//upperbodycascade.load( "haarcascade_upperbody.xml" ) ;
facecascade.load( "haarcascade_frontalface_alt.xml" ) ;
eyecascade.load( "haarcascade_eye.xml" ) ;

// Start Video..1) 0 for WebCam 2) "Path to Video" for a Local Video
capture.open(0);
if( !capture.isOpened() )
{
cout << "Camera port opening failed!" << endl;
exit(1);
}
else
{
cout << "Camera port opened successfully!" << endl;
}
// set resolution & frame rate (FPS)
capture.set(CAP_PROP_FRAME_WIDTH, 640);
capture.set(CAP_PROP_FRAME_HEIGHT,480);
//capture.set(CAP_PROP_FPS, 30);

while(1)
{
cout << "####reading frame" << endl;
capture >> frame;
if( frame.empty() )
break;
Mat frame1 = frame.clone();
//detectAndDisplay( frame1, fullbodycascade, upperbodycascade);
detectAndDraw(frame1, facecascade, eyecascade, scale);
waitKey(1);
}
capture.release();
return 0;
}

/*void detectAndDisplay( Mat& frame, CascadeClassifier& fullbodycascade, CascadeClassifier& upperbodycascade)
{
std::vector<Rect> upperbodies, fullbodies;
Mat frame_gray;

cvtColor(frame, frame_gray, COLOR_BGR2GRAY);
equalizeHist(frame_gray, frame_gray);

//-- Detect upperbody
upperbodycascade.detectMultiScale(frame_gray, upperbodies, 1.1, 3, 0 | CASCADE_SCALE_IMAGE, Size(30, 30));

cout << "upperbody size: " << upperbodies.size() << endl;
for (size_t i = 0; i < upperbodies.size(); i++)
{
rectangle(frame, upperbodies[i], Scalar(255, 0, 255), 1, 8, 0);

//-- Detect fullbody
fullbodycascade.detectMultiScale(frame_gray, fullbodies, 1.1, 3, 0 | CASCADE_SCALE_IMAGE, Size(30, 30));
cout << "full body size: " << fullbodies.size() << endl;
for (size_t i = 0; i < fullbodies.size(); i++)
{
rectangle(frame, fullbodies[i], Scalar(255, 0, 255), 1, 8, 0);
}
}

//-- Show what you got
imshow("pedestrian detection", frame);
}*/

void detectAndDraw( Mat& img, CascadeClassifier& cascade,
CascadeClassifier& nestedCascade, double scale)
{
vector<Rect> faces;
Mat gray; //smallImg;

cvtColor( img, gray, COLOR_BGR2GRAY ); // Convert to Gray Scale
//double fx = 1 / scale;

// Resize the Grayscale Image
//resize( gray, smallImg, Size(), fx, fx, INTER_LINEAR );
equalizeHist( gray, gray );

// Detect faces of different sizes using cascade classifier
cascade.detectMultiScale(gray, faces, 1.1,
3, 0|CASCADE_SCALE_IMAGE, Size(30, 30));

cout << "face size: " << faces.size() << endl;
// Draw circles around the faces
for ( size_t i = 0; i < faces.size(); i++ )
{
Rect r = faces[i];
Mat smallImgROI;
vector<Rect> nestedObjects;
Point center;
Scalar color = Scalar(255, 0, 0); // Color for Drawing tool
int radius;

double aspect_ratio = (double)r.width/r.height;
if( 0.75 < aspect_ratio && aspect_ratio < 1.3 )
{
center.x = cvRound((r.x + r.width*0.5)*scale);
center.y = cvRound((r.y + r.height*0.5)*scale);
radius = cvRound((r.width + r.height)*0.25*scale);
circle( img, center, radius, color, 3, 8, 0 );
}
else
rectangle( img, cv::Point(cvRound(r.x*scale), cvRound(r.y*scale)),
cv::Point(cvRound((r.x + r.width-1)*scale),
cvRound((r.y + r.height-1)*scale)), color, 3, 8, 0);
if( nestedCascade.empty() )
continue;
smallImgROI = gray( r );

// Detection of eyes int the input image
nestedCascade.detectMultiScale( smallImgROI, nestedObjects, 1.1, 3,
0|CASCADE_SCALE_IMAGE, Size(30, 30) );

// Draw circles around eyes
for ( size_t j = 0; j < nestedObjects.size(); j++ )
{
Rect nr = nestedObjects[j];
center.x = cvRound((r.x + nr.x + nr.width*0.5)*scale);
center.y = cvRound((r.y + nr.y + nr.height*0.5)*scale);
radius = cvRound((nr.width + nr.height)*0.25*scale);
circle( img, center, radius, color, 3, 8, 0 );
}
}

// Show Processed Image with detected faces
imshow( "Face Detection", img );
}

/*void detectAndDraw( Mat& image, CascadeClassifier& face_cascade)
{
// Detect faces
std::vector<Rect> faces;
face_cascade.detectMultiScale( image, faces, 1.1, 2, 0|CASCADE_SCALE_IMAGE, Size(30, 30) );

cout << "body size: " << faces.size() << endl;
// Draw circles on the detected faces
for( unsigned int i = 0; i < faces.size(); i++ )
{
Point center( faces[i].x + faces[i].width*0.5, faces[i].y + faces[i].height*0.5 );
ellipse( image, center, Size( faces[i].width*0.5, faces[i].height*0.5), 0, 0, 360, Scalar( 255, 0, 255 ), 4, 8, 0 );
}
imshow( "Detected Face", image );
}*/

0 Kudos

10,816 Views
manish_bajaj
NXP Employee
NXP Employee

nxf60449‌,

Please check this ticket.

-Manish

0 Kudos

10,816 Views
Alifer_Moraes
NXP Employee
NXP Employee

Hello,

Object Detection using Haar feature-based cascade classifiers is relatively slow by nature. There is no GPU optimization for it.

However, trying to resize frames used in the methods detectMultiScale to a smaller size may improve performance.

Alifer

0 Kudos

10,816 Views
manish_bajaj
NXP Employee
NXP Employee

Above example should work for i.MX8M too, you can refer C++ example from below link

https://source.codeaurora.org/external/imx/tensorflow-imx/tree/tensorflow/lite/examples/label_image

-Manish

10,816 Views
manizillion
Contributor IV

Hi Manish,

I see my object detection application with veryslow response on imx8mqevk , i have done the following configurations for vivante , do i miss anything to speedup camera apps ?

# Graphics libraries
PREFERRED_PROVIDER_virtual/egl ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libgl ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libgles1 ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libgles2 ?= "imx-gpu-viv"

PREFERRED_PROVIDER_virtual/egl_imxgpu ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libgl_imxgpu3d ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libgles1_imxgpu3d ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libgles2_imxgpu3d ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libg2d ?= "imx-gpu-viv"
PREFERRED_PROVIDER_virtual/libg2d_imxdpu ?= "imx-dpu-viv"

0 Kudos

10,816 Views
manish_bajaj
NXP Employee
NXP Employee

Manivannan,

Please check below link. It have lot of sample application and enables GPU.

https://source.codeaurora.org/external/imxsupport/pyeiq

For TFLite we use NNAPI delegates to support GPU. For application based on TFLite use UseNNAPI(TRUE) to enable GPU.

-Manish

0 Kudos

10,816 Views
manizillion
Contributor IV

thanks Manish,  Any reference available for imx8mq , looks like the link you shared is not for this imx8 chipset.

0 Kudos

10,816 Views
manizillion
Contributor IV

thanks Manish,

Can you share the any cpp code base for the same GPU enable run. This was on py ..

0 Kudos

10,816 Views
manish_bajaj
NXP Employee
NXP Employee

You should be able to use Open CV based application on i.MX8MQ. Refer below link for sample example. 

https://source.codeaurora.org/external/imxsupport/pyeiq

0 Kudos

10,816 Views
ullasbharadwaj
Contributor III

Hello Manish,

Does it run on GPU? I am using i.MX8 qmmek but openCV application does not run on GPU.

Best Regards

Ullas Bharadwaj

0 Kudos

10,816 Views
manish_bajaj
NXP Employee
NXP Employee

ML using OpenCV framework is not accelerated on GPU. Though some one can create application on openCV. There are other component  like gstreamer and other component which can be hardware accelerated. Above link provide example of using OpenCV using Python.

-Manish 

0 Kudos

10,817 Views
manizillion
Contributor IV

Manish,

how to port any application to run on GPU, any info on that will be helpfull