Image Classification example of TF-lite do not use GPU on iWG27M iMX8QM kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Image Classification example of TF-lite do not use GPU on iWG27M iMX8QM kit

ソリューションへジャンプ
4,227件の閲覧回数
kushal_chaudhar
Contributor I

Hi

I tested  the Image classification example given in UM11226 section 7.2 On iWG27M iMX8QM SOM development kit, with Yocto ML manifest having 4.9.51 beta kernel with Opencl support.

It works fine and predicts the results in around 300 ms but it does not uses GPU. gputop application do not show any process running.

So My questions are

1) Why the application is not using GPU for its execution? (In spite of OpenCL support).

2) What needs to be done to use the GPU support.

3) I need TensorFlow-lite object detection example which utilize GPU for its execution, where Can I find that?

ラベル(1)
0 件の賞賛
1 解決策
3,868件の閲覧回数
vanessa_maegima
NXP Employee
NXP Employee

Hi [email protected]‌,

There's no GPU support on eIQ yet.

Thanks,

Vanessa

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
3,868件の閲覧回数
simple_do
Contributor I

Hi Vanessa Maegima:

      there is example for tf-lite on  gpu run, it's avalible.

pastedImage_1.png

0 件の賞賛
3,869件の閲覧回数
vanessa_maegima
NXP Employee
NXP Employee

Hi [email protected]‌,

There's no GPU support on eIQ yet.

Thanks,

Vanessa

0 件の賞賛