Converting a Keras model for eIQ use

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Converting a Keras model for eIQ use

Converting a Keras model for eIQ use

NXP BSP currently does not support running a Keras application directly on i.MX. The customers that use this approach must convert their Keras model into one the supported inference engines in eIQ. In this post we will cover converting a Keras model (.h5) to a TfLite model (.tflite).

  • Install TensorFlow with the same eIQ TfLite supported version (you can find this information on Linux User's Guide). For L4.19.35_1.0.0 the TfLite version is v1.12.0.

$ pip3 install tensorflow==1.12.0

  • Run the following commands in a python3 environment to convert the .h5 model to a .tflite model:

>>> from tensorflow.contrib import lite
>>> converter = lite.TFLiteConverter.from_keras_model_file('model.h5') #path to your model 
>>> tfmodel = converter.convert()
>>> open("model.tflite", "wb").write(tfmodel)

The model can be deployed and used by TfLite inference engine in eIQ.

Labels (1)
Comments

Execute the following command to also convert the Keras mobilenet.h5 model to the mobilenet.tflite model:

eiq-converter --plugin eiq-converter-tflite mobilenet.h5 mobilenet.tflite

No ratings
Version history
Last update:
‎03-13-2020 10:57 AM
Updated by: