Building eIQ image failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building eIQ image failed

3,826 Views
g0930421313
Contributor II

Hi

I'm building an eIQ image for my imx8mqevk and encountered following  error log cause a build failed.
Before that I have followed the User Manual "UM11226"  step by step, soon i met a COMPATIBLE_MACHINE Error and edit the end of meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb  file

from  COMPATIBLE_MACHINE = "(imx8qm)"

to COMPATIBLE_MACHINE = "(imx8qm|imx8mqevk)" solve this issue successfully.

what should i do?

OS : Ubuntu16.04 in VMWare Workstation 15 Player

 

NOTE: Your conf/bblayers.conf has been automatically updated.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:05:48
Parsing of 2577 .bb files complete (0 cached, 2577 parsed). 3499 targets, 221 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: Multiple providers are available for runtime ptpd (ptpd, ptpd-qoriq)
Consider defining a PREFERRED_RPROVIDER entry to match ptpd
NOTE: Multiple providers are available for runtime ptpd-dev (ptpd, ptpd-qoriq)
Consider defining a PREFERRED_RPROVIDER entry to match ptpd-dev

Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mqevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-poky = "HEAD:c9bd4984f8f471ca2c43052714f4413ba99cf171"
meta-oe
meta-multimedia = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-freescale = "HEAD:27ca94f8a4336790ba117b4298566f6820e7e74c"
meta-freescale-3rdparty = "HEAD:82037216280a39957fb4272581637abec734ad50"
meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"
meta-bsp
meta-sdk = "HEAD:8eeb420fad668b733ab95b460895e1c337c66b25"
meta-browser = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-qt5 = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"
meta-imx-machinelearning = "HEAD:7e9294dead55d1f6b4f1cfe486e0c4e0c5097953"

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:19
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: nspr-native-4.19-r0 do_fetch: Failed to fetch URL http://ftp.mozilla.org/pub/nspr/releases/v4.19/src/nspr-4.19.tar.gz , attempting MIRRORS if available
WARNING: nss-native-3.35-r0 do_fetch: Failed to fetch URL http://ftp.mozilla.org/pub/mozilla.org/security/nss/releases/NSS_3_35_RTM/src/nss-3.35.tar.gz , attempting MIRRORS if available
WARNING: mesa-2_17.3.8-r0 do_fetch: Failed to fetch URL https://mesa.freedesktop.org/archive/mesa-17.3.8.tar.xz , attempting MIRRORS if available
WARNING: icu-native-60.2-r0 do_fetch: Checksum mismatch for local file /home/stu/fsl-arm-yocto-bsp/downloads/icu4c-60_2-src.tgz
Cleaning and trying again.
WARNING: icu-native-60.2-r0 do_fetch: Renaming /home/stu/fsl-arm-yocto-bsp/downloads/icu4c-60_2-src.tgz to /home/stu/fsl-arm-yocto-bsp/downloads/icu4c-60_2-src.tgz_bad-checksum_e869986174e1719338a3baf5b95ca4f2
WARNING: icu-native-60.2-r0 do_fetch: Checksum failure encountered with download of http://download.icu-project.org/files/icu4c/60.2/icu4c-60_2-src.tgz  - will attempt other sources if available
WARNING: leptonica-1.74.4-r0 do_fetch: Checksum mismatch for local file /home/stu/fsl-arm-yocto-bsp/downloads/leptonica-1.74.4.tar.gz
Cleaning and trying again.
WARNING: leptonica-1.74.4-r0 do_fetch: Renaming /home/stu/fsl-arm-yocto-bsp/downloads/leptonica-1.74.4.tar.gz to /home/stu/fsl-arm-yocto-bsp/downloads/leptonica-1.74.4.tar.gz_bad-checksum_294113120dc2d94ae2f9555eea7f0bd0
WARNING: leptonica-1.74.4-r0 do_fetch: Checksum failure encountered with download of http://leptonica.com/source/leptonica-1.74.4.tar.gz  - will attempt other sources if available
WARNING: opencv-4.0.1+gitAUTOINC+c9ad5779f2_2522124473_32e315a5b1_34e4206aef_fccf7cd6a4_d29d003e00-r0 do_configure: QA Issue: opencv: invalid PACKAGECONFIG: neon [invalid-packageconfig]
WARNING: libeigen-3.3.4-r0 do_fetch: Failed to fetch URL http://bitbucket.org/eigen/eigen/get/3.3.4.tar.bz2;downloadfilename=libeigen-3.3.4.tar.bz2 , attempting MIRRORS if available
WARNING: nbench-byte-2.2.3-r0 do_fetch: Failed to fetch URL https://fossies.org/linux/misc/nbench-byte-2.2.3.tar.gz , attempting MIRRORS if available
WARNING: sudo-1.8.22-r0 do_fetch: Failed to fetch URL http://ftp.sudo.ws/sudo/dist/sudo-1.8.22.tar.gz , attempCurrently 2 running tasks (5388 of 8934) 60% |#####################################################WARNING: lttng-modules-2.10.6-r0 do_package: lttng-modules: no modules were created; this may be due to CONFIG_TRACEPOINTS not being enabled in your kernel.
ERROR: tensorflow-1.12.0-r0 do_configure: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)
ERROR: Logfile of failure stored in: /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900
Log data follows:
| DEBUG: Executing shell function do_configure
| downloading https://bitbucket.org/eigen/eigen/get/fd6845384b86.tar.gz 
|
| gzip: stdin: unexpected end of file
| tar: Child returned status 1
| tar: Error is not recoverable: exiting now
| WARNING: exit code 2 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /home/stu/fsl-arm-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow/1.12.0-r0/temp/log.do_configure.84900)
ERROR: Task (/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6041 tasks of which 0 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/stu/fsl-arm-yocto-bsp/sources/meta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb:do_configure
Summary: There were 14 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

 
Labels (1)
0 Kudos
3 Replies

3,509 Views
RajuKoppada
Contributor I

Hi @g0930421313 ,

 

Did you fix this issue? I am also seeing same issue and I am working on imx 8m quadmax platform.

If you have a fix for please help me on this.

 

Thanks and Regards,

Raju

 

 

 

0 Kudos

3,816 Views
强王
Contributor IV

很明显eigen下载失败了

0 Kudos

3,800 Views
g0930421313
Contributor II

Hi

請問下載失敗的原因可能是什麼?

我可以確定我的網路是沒問題的......

Thanks!

Best Regards

0 Kudos