Zephyr support for S32K388 Evaluation Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zephyr support for S32K388 Evaluation Board

ソリューションへジャンプ
653件の閲覧回数
dianaT
Contributor I

Hello NXP team,

I'm currently working with the S32K388EVB-Q289 Evaluation Board and was wondering if there are any plans to add official support for it in the Zephyr project.

I've seen that Zephyr already supports the S32k344 MCU, but since the S32K388 has additional features (such as more cores, bigger memory and extra peripherals), it seems that the existing S32K344 support wouldn't be directly compatible or sufficient for S32K388.
Before attempting to integrate it myself, I wanted to check if there is any internal roadmap or upcoming release that includes support for the S32K388 and this evaluation board.

Thanks in advance for your time and help!

S32K3 ZEPHYR-OS-EDGE S32K3X8EVB-Q289

タグ(2)
0 件の賞賛
返信
1 解決策
603件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport


Hi,

Thank you for your interest in our products and for contributing to our community.

I see you have another thread about the same issue in Zephyr project:

https://github.com/zephyrproject-rtos/zephyr/discussions/92467#discussioncomment-13638974

Please continue discussion such forum, where experts on the subject can help you.

We appreciate your understanding.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
604件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport


Hi,

Thank you for your interest in our products and for contributing to our community.

I see you have another thread about the same issue in Zephyr project:

https://github.com/zephyrproject-rtos/zephyr/discussions/92467#discussioncomment-13638974

Please continue discussion such forum, where experts on the subject can help you.

We appreciate your understanding.

0 件の賞賛
返信