Using MCUboot RAM loading with Zephyr for i.MX RT1060

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using MCUboot RAM loading with Zephyr for i.MX RT1060

1,014 次查看
ildiko_pocsai
Contributor I

I’m currently trying to get the RAM loading working with MCUboot in Zephyr for i.MX RT1060 but I’m not able to make the bootloader boot the image. Here are the steps I did so far:

  • In "samples/sysbuild/with_mcuboot/sysbuild.conf", added SB_CONFIG_MCUBOOT_MODE_RAM_LOAD=y.
  • Set CONFIG_SRAM_SIZE=128 in samples/sysbuild/with_mcuboot-sysbuild/mcuboot.conf.

In the generated .config file I can see that the CONFIG_SRAM_BASE_ADDRESS=0x80000000 which seems to be correct. But MCUboot reports the error message "Unable to find bootable image" instead of starting the application.

I'm using the Zephyr release 4.1.0.

Do I need to make any other changes?

Thanks.

Ildikó

0 项奖励
回复
4 回复数

716 次查看
dereksnell
NXP Employee
NXP Employee

FYI  @ildiko_pocsai and @Omar_Anguiano ,

This article has steps and Git patches to enable RAM Loading on the RT1060 EVK, see https://community.nxp.com/t5/Zephyr-Project-Knowledge-Base/MCUboot-RAM-Loading-with-Zephyr/ta-p/2139...  .

Best regards

0 项奖励
回复

921 次查看
ildiko_pocsai
Contributor I

Hello Omar,

Thanks for your reply. Yes, I want to use the external SDRAM. Can you please explain me how to add the DCD to the image in Zephyr. I'm using Zephyr's sysbuild build system to build MCUboot and my application which uses the MCUboot imgtool to sign the image. But I cannot find any option for the imgtool to add the DCD.

Thanks.

Ildikó

0 项奖励
回复

884 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

You can use a tool such as Secure Provisioning Tool or MCUBootUtility to add the DCD to the image, from the binary generated, the dcd can be added. If you don’t have already a dcd then you can generate it in ConfigTools.

Best regards,
Omar

0 项奖励
回复

957 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello, I hope you are well. 
Address 0x80000000 is for external SDRAM, do you want to load the image to that SDRAM? IF that is the case, then you will need to add to your image the DCD so the SDRAM is initialized during boot, so when code is moved to the SDRAM, it is ready to execute. 

Best regards,
Omar

0 项奖励
回复