SD tuning failed on configuring to SDR50 in IMXRT1060

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD tuning failed on configuring to SDR50 in IMXRT1060

1,067 次查看
Jack007
Contributor III

Hello,

I am trying to bring up the Zephyr on imxrt1060 with Murata module but on configuring sdio speed to SDR50 SDIO enumeration Fails by stating SD tunning failed.

Below is the error log:

[00:00:02.819,000] <dbg> usdhc: imx_usdhc_set_io: SDHC I/O: bus width 4, clock 400000Hz, card power ON, voltage 1.8V
[00:00:02.819,000] <err> sd: Raised card bus width to 4 bits
[00:00:02.819,000] <err> sd: Select and set bus speed
[00:00:02.835,000] <dbg> sd: sdio_set_bus_speed: Setting bus clock to: 100000000
[00:00:02.835,000] <dbg> usdhc: imx_usdhc_set_io: SDHC I/O: bus width 4, clock 100000000Hz, card power ON, voltage 1.8V
[00:00:02.836,000] <dbg> usdhc: imx_usdhc_set_io: BUS CLOCK: 99000000
[00:00:02.864,000] <err> usdhc: imx_usdhc_transfer USDHC_TransferNonBlocking kStatus_USDHC_ReTuningRequest error :6505
[00:00:02.864,000] <err> usdhc: imx_usdhc_execute_tuning imx_usdhc_transfer ret :-11
[00:00:02.864,000] <err> sd: SD tuning failed: -11

on further debug found that USDHC_TransferNonBlocking is failing by returns kStatus_USDHC_ReTuningRequest

Can please help in solving this issue.

NOTE: I don't see any issue on configuring SDR12 and SDR25. 

0 项奖励
回复
1 回复

1,028 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Jack007,

I believe this is a duplicated post from the one you posted on the i.MX Processors forum here: SD tuning Fails with MIMXRT1060. - NXP Community

In order to prevent double efforts, I will continue supporting you on the aforementioned post exclusively.

Thank you for your understanding.

BR,
Edwin.

0 项奖励
回复