The NXP zsdk information specifies that RW612 supports scantternet topology, which allows for a peripheral to be connected to multiple centrals nxp-zsdk/doc/wireless/release-notes/topics/bluetooth_radio_features.md at main · nxp-zephyr/nxp-zsdk....
How many connections are supported from a peripheral device to different BLE centrals?Are there any constraints across these connections? Shall they use same PHY, connection parameters or other traits ?Best regards Tonny Bing
Hello,
Hope you are doing well.
For our examples, we have the
CONFIG_BT_MAX_CONN=16
This match the "Maximum 16 Bluetooth LE connections" from the Relese Notes.
Regards,
Ricardo
You may check the datasheet for different topology.There are one antenna topology and two antenna topology using internal SPDT