MCUBoot and Edgelock Secure Enclave on an MCXN947 using Zephyr

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUBoot and Edgelock Secure Enclave on an MCXN947 using Zephyr

ソリューションへジャンプ
1,063件の閲覧回数
ClarkS
Contributor III

I would like to use Zephyr's open source MCUBoot module on an IoT project using the FRDM-MCXN947 board, but also use the Edgelock Secure Enclave to increase key security. Am I correct that this would be difficult because it would require modification of MCUBoot source in order to get MCUBoot to use the Secure Enclave? 

If I am correct about this, is it likely Zephyr / MCUBoot will use the Edgelock secure enclave in the future? 

Am I correct that this improvement would provide a significant increase in security? Or should I be content with the key handling in standard Zephyr MCUBoot?

0 件の賞賛
返信
1 解決策
1,038件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @ClarkS 

Yes, i think using EdgeLock SE with MCUBoot is currently not trivial and would require source modifications or a custom integration layer.

I will forward your requirements to our relevant team. Thank you for your suggestion.

BR

Harry

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,039件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @ClarkS 

Yes, i think using EdgeLock SE with MCUBoot is currently not trivial and would require source modifications or a custom integration layer.

I will forward your requirements to our relevant team. Thank you for your suggestion.

BR

Harry

0 件の賞賛
返信
862件の閲覧回数
ClarkS
Contributor III

@Harry_Zhang Do you have any feedback on if or when this might be accomplished? If it’s not soon, do you have any suggestions on how to use MCUBoot in Zephyr and maintain the best key security?

Best wishes.!

Clark

0 件の賞賛
返信