Zephyr resources for Peripherals and drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zephyr resources for Peripherals and drivers

Zephyr resources for Peripherals and drivers

If you have any questions or issues related to these resources, please Ask a new question, and the NXP support team can address it there.

One of the popular reasons developers choose Zephyr is the large offering of drivers and peripheral support.  The best place to look for the latest drivers and features supported on a hardware platform, is on the board’s documentation page.  For example, this Supported Features table lists the latest support for the FRDM-MCXN947 board.  Here are the links to these pages for all the boards with Zephyr support.

NXP’s Hardware Abstraction Layer (HAL) is based on the MCUXpresso SDK drivers.  To learn more, see the blog Zephyr Software Code Reuse with NXP MCUXpresso SDK.  Most users want to use the Zephyr driver APIs in their application for portability.  But if a Zephyr driver is not supported on a platform, or if there is no Zephyr driver for a hardware peripheral, another option is Using MCUXpresso SDK drivers in Zephyr app.

Peripheral Clocks: Most peripheral clocks are enabled in SOC or board source files, see Clock Configuration in Zephyr.  One common issue Zephyr users have when enabling or adding a peripheral instance on their board, is that instance is not clocked properly.  Below are some helpful resources for specific peripherals and drivers:

Accelerators and Coprocessors

Analog to Digital Converter (ADC)

Displays

  • Most displays are enabled in Zephyr as shields, which are add-on hardware modules.  See Zephyr’s list of shields.
  • Typically a board page will document a display shield it has been tested with.  For example, the FRDM-MCXN947 board page includes the LCD_PAR_S035 display shield.
  • The shield page gives instructions how to include that shield in the build, and add to the application.  For example, see the LCD_PAR_S035 shield page.  If building with VS Code, see the CMake wiki
  • Zephyr has a couple samples that use displays, including the display driver sample and the LVGL demo.

Direct Memory Access (DMA)

  • When using a DMA, be aware of cache coherency, and make sure buffers accessed by DMA are not in cacheable memory.  This includes when using other drivers that use DMA, like I2S, SPI, UART, etc..  A good reference for placing buffers in non-cacheable memory is the spi_loopback test.

Inter-Integrated Circuit (I2C)

The Zephyr repo has a couple I2C sample applications, but because these depend on I2C targets in hardware, these samples are enabled on a small number of boards.  Here is a list of other I2C references:

  • i2c_target_api test – this is the primary test NXP uses to test I2C on the supported boards.  This is a loopback test using two I2C peripherals.  One is configured as a controller, and the other as a target which emulates an EEPROM.  For this test to pass, usually the I2C signals must be shorted to connect the two I2Cs.  For the list of supported boards, see the testcase.yaml.
  • Sensor samples – many NXP evaluation boards include sensors on the I2C bus.  Depending on the board, there may be some sensor sample apps.  For example, the accelerometer trigger and accelerometer polling samples are supported on many NXP boards.  For the list of supported boards, see the accel_trig/boards folder or the accel_polling sample.yaml.
  • I2c_shell – this is not a sample app, but a shell feature that is easy to add to an app.  If there is no driver or example available to communicate with an I2C target, this feature can be helpful to test out the communication.  Through the shell, I2C controllers can scan for targets and send read/write commands to them.  Golioth shared this great blog on i2c_shell with all the details. 

Inter-Integrated Circuit Sound (I2S)

  • The I2S drivers are tested using Zephyr’s i2s_speed test.  That is a loopback test, and some boards require changes to connect the signals for the test to pass, see the readme.

Networking

includes Ethernet

Serial Peripheral Interface (SPI)

Universal Serial Bus (USB)

 

Return to Zephyr Knowledge Hub

%3CLINGO-SUB%20id%3D%22lingo-sub-2008589%22%20slang%3D%22en-US%22%20mode%3D%22UPDATE%22%3EZephyr%20resources%20for%20Peripherals%20and%20drivers%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2008589%22%20slang%3D%22en-US%22%20mode%3D%22UPDATE%22%3E%0A%3CP%3E%3CSPAN%3EIf%20you%20have%20any%20questions%20or%20issues%20related%20to%20these%20resources%2C%20please%26nbsp%3B%3C%2FSPAN%3E%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project%2Fbd-p%2FZephyr-Project%22%20target%3D%22_blank%22%3EAsk%20a%20new%20question%3C%2FA%3E%3CSPAN%3E%2C%20and%20the%20NXP%20support%20team%20can%20address%20it%20there.%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EOne%20of%20the%20popular%20reasons%20developers%20choose%20Zephyr%20is%20the%20large%20offering%20of%20drivers%20and%20peripheral%20support.%26nbsp%3B%20The%20best%20place%20to%20look%20for%20the%20latest%20drivers%20and%20features%20supported%20on%20a%20hardware%20platform%2C%20is%20on%20the%20board%E2%80%99s%20documentation%20page.%26nbsp%3B%20For%20example%2C%20this%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fboards%2Fnxp%2Ffrdm_mcxn947%2Fdoc%2Findex.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ESupported%20Features%3C%2FA%3E%20table%20lists%20the%20latest%20support%20for%20the%20FRDM-MCXN947%20board.%26nbsp%3B%20Here%20are%20the%20links%20to%20these%20pages%20for%20all%20the%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fboards%2Fnxp%2Findex.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Eboards%20with%20Zephyr%20support%3C%2FA%3E.%3C%2FP%3E%0A%3CP%3ENXP%E2%80%99s%20Hardware%20Abstraction%20Layer%20(HAL)%20is%20based%20on%20the%20MCUXpresso%20SDK%20drivers.%26nbsp%3B%20To%20learn%20more%2C%20see%20the%20blog%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fcompany%2Fabout-nxp%2Fsmarter-world-blog%2FBL-ZEPHYR-SOFTWARE-CODE%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EZephyr%20Software%20Code%20Reuse%20with%20NXP%20MCUXpresso%20SDK%3C%2FA%3E.%26nbsp%3B%20Most%20users%20want%20to%20use%20the%20Zephyr%20driver%20APIs%20in%20their%20application%20for%20portability.%26nbsp%3B%20But%20if%20a%20Zephyr%20driver%20is%20not%20supported%20on%20a%20platform%2C%20or%20if%20there%20is%20no%20Zephyr%20driver%20for%20a%20hardware%20peripheral%2C%20another%20option%20is%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project-Knowledge-Base%2FUsing-MCUXpresso-SDK-drivers-in-a-Zephyr-application%2Fta-p%2F2077778%22%20target%3D%22_blank%22%3EUsing%20MCUXpresso%20SDK%20drivers%20in%20Zephyr%20app%3C%2FA%3E.%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3EPeripheral%20Clocks%3C%2FSTRONG%3E%3A%20Most%20peripheral%20clocks%20are%20enabled%20in%20SOC%20or%20board%20source%20files%2C%20see%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project-Knowledge-Base%2FClock-Configuration-in-Zephyr%2Fta-p%2F2166958%22%20target%3D%22_self%22%3EClock%20Configuration%20in%20Zephyr%3C%2FA%3E.%26nbsp%3B%20One%20common%20issue%20Zephyr%20users%20have%20when%20enabling%20or%20adding%20a%20peripheral%20instance%20on%20their%20board%2C%20is%20that%20instance%20is%20not%20clocked%20properly.%26nbsp%3B%20Below%20are%20some%20helpful%20resources%20for%20specific%20peripherals%20and%20drivers%3A%3C%2FP%3E%0A%3CH2%20id%3D%22toc-hId--557348464%22%20id%3D%22toc-hId--499197463%22%3EAccelerators%20and%20Coprocessors%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F72195%23discussioncomment-9501252%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EPowerQuad%3C%2FA%3E%3C%2FLI%3E%0A%3CLI%3EAppnote%20%3CA%20href%3D%22https%3A%2F%2Fdocs.nxp.com%2Fbundle%2FAN13970%2Fpage%2Ftopics%2Fintroduction.html%3F_gl%3D1*13k6mj2*_ga*NjYxNDQ2MTAzLjE3MTg2MzQyNzE.*_ga_WM5LE0KMSH*MTczMzQzMDcyMy4zODQuMS4xNzMzNDMyMDQ4LjAuMC4w%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN13970%3C%2FA%3E%20Running%20Zephyr%20RTOS%20on%20Cadence%20Tensilica%20HiFi%204%20DSP%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId-1930164369%22%20id%3D%22toc-hId-1988315370%22%3EAnalog%20to%20Digital%20Converter%20(ADC)%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3EZephyr%20sample%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Ftree%2Fmain%2Fsamples%2Fsensor%2Fdie_temp_polling%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Edie_temp_polling%3C%2FA%3E%20to%20measure%20temperature%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId-122709906%22%20id%3D%22toc-hId-180860907%22%3EDisplays%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3EMost%20displays%20are%20enabled%20in%20Zephyr%20as%20shields%2C%20which%20are%20add-on%20hardware%20modules.%26nbsp%3B%20See%20Zephyr%E2%80%99s%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fboards%2Findex.html%23shields%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Elist%20of%20shields%3C%2FA%3E.%3C%2FLI%3E%0A%3CLI%3ETypically%20a%20board%20page%20will%20document%20a%20display%20shield%20it%20has%20been%20tested%20with.%26nbsp%3B%20For%20example%2C%20the%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fboards%2Fnxp%2Ffrdm_mcxn947%2Fdoc%2Findex.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EFRDM-MCXN947%20board%20page%3C%2FA%3E%20includes%20the%20LCD_PAR_S035%20display%20shield.%3C%2FLI%3E%0A%3CLI%3EThe%20shield%20page%20gives%20instructions%20how%20to%20include%20that%20shield%20in%20the%20build%2C%20and%20add%20to%20the%20application.%26nbsp%3B%20For%20example%2C%20see%20the%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fboards%2Fshields%2Flcd_par_s035%2Fdoc%2Findex.html%23lcd-par-s035%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ELCD_PAR_S035%20shield%20page%3C%2FA%3E.%26nbsp%3B%20If%20building%20with%20VS%20Code%2C%20see%20the%20%3CA%20href%3D%22https%3A%2F%2Fmcuxpresso.nxp.com%2Fmcux-vscode%2Flatest%2Fhtml%2FCMake.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ECMake%20wiki%3C%2FA%3E.%26nbsp%3B%3C%2FLI%3E%0A%3CLI%3EZephyr%20has%20a%20couple%20samples%20that%20use%20displays%2C%20including%20the%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fsamples%2Fdrivers%2Fdisplay%2FREADME.html%23display%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Edisplay%20driver%20sample%3C%2FA%3E%20and%20the%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fsamples%2Fmodules%2Flvgl%2Fdemos%2FREADME.html%23lvgl-demos%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ELVGL%20demo%3C%2FA%3E.%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId--1684744557%22%20id%3D%22toc-hId--1626593556%22%3EDirect%20Memory%20Access%20(DMA)%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3EWhen%20using%20a%20DMA%2C%20be%20aware%20of%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F61966%23discussioncomment-6846802%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Ecache%20coherency%3C%2FA%3E%2C%20and%20make%20sure%20buffers%20accessed%20by%20DMA%20are%20not%20in%20cacheable%20memory.%26nbsp%3B%20This%20includes%20when%20using%20other%20drivers%20that%20use%20DMA%2C%20like%20I2S%2C%20SPI%2C%20UART%2C%20etc..%20%26nbsp%3BA%20good%20reference%20for%20placing%20buffers%20in%20non-cacheable%20memory%20is%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Ftree%2Fmain%2Ftests%2Fdrivers%2Fspi%2Fspi_loopback%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Espi_loopback%20test%3C%2FA%3E.%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId-802768276%22%20id%3D%22toc-hId-860919277%22%3EInter-Integrated%20Circuit%20(I2C)%3C%2FH2%3E%0A%3CP%3EThe%20Zephyr%20repo%20has%20a%20couple%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fsamples%2Fdrivers%2Fi2c%2FREADME.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EI2C%20sample%20applications%3C%2FA%3E%2C%20but%20because%20these%20depend%20on%20I2C%20targets%20in%20hardware%2C%20these%20samples%20are%20enabled%20on%20a%20small%20number%20of%20boards.%26nbsp%3B%20Here%20is%20a%20list%20of%20other%20I2C%20references%3A%3C%2FP%3E%0A%3CUL%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fblob%2Fmain%2Ftests%2Fdrivers%2Fi2c%2Fi2c_target_api%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Ei2c_target_api%20test%3C%2FA%3E%20%E2%80%93%20this%20is%20the%20primary%20test%20NXP%20uses%20to%20test%20I2C%20on%20the%20supported%20boards.%26nbsp%3B%20This%20is%20a%20loopback%20test%20using%20two%20I2C%20peripherals.%26nbsp%3B%20One%20is%20configured%20as%20a%20controller%2C%20and%20the%20other%20as%20a%20target%20which%20emulates%20an%20EEPROM.%26nbsp%3B%20For%20this%20test%20to%20pass%2C%20usually%20the%20I2C%20signals%20must%20be%20shorted%20to%20connect%20the%20two%20I2Cs.%26nbsp%3B%20For%20the%20list%20of%20supported%20boards%2C%20see%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fblob%2Fmain%2Ftests%2Fdrivers%2Fi2c%2Fi2c_target_api%2Ftestcase.yaml%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Etestcase.yaml%3C%2FA%3E.%3C%2FLI%3E%0A%3CLI%3ESensor%20samples%20%E2%80%93%20many%20NXP%20evaluation%20boards%20include%20sensors%20on%20the%20I2C%20bus.%26nbsp%3B%20Depending%20on%20the%20board%2C%20there%20may%20be%20some%20sensor%20sample%20apps.%26nbsp%3B%20For%20example%2C%20the%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fsamples%2Fsensor%2Faccel_trig%2FREADME.html%23accel_trig%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Eaccelerometer%20trigger%3C%2FA%3E%20and%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fsamples%2Fsensor%2Faccel_polling%2FREADME.html%23accel_polling%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Eaccelerometer%20polling%3C%2FA%3E%20samples%20are%20supported%20on%20many%20NXP%20boards.%26nbsp%3B%20For%20the%20list%20of%20supported%20boards%2C%20see%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Ftree%2Fmain%2Fsamples%2Fsensor%2Faccel_trig%2Fboards%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Eaccel_trig%2Fboards%20folder%3C%2FA%3E%20or%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fblob%2Fmain%2Fsamples%2Fsensor%2Faccel_polling%2Fsample.yaml%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Eaccel_polling%20sample.yaml%3C%2FA%3E.%3C%2FLI%3E%0A%3CLI%3EI2c_shell%20%E2%80%93%20this%20is%20not%20a%20sample%20app%2C%20but%20a%20shell%20feature%20that%20is%20easy%20to%20add%20to%20an%20app.%26nbsp%3B%20If%20there%20is%20no%20driver%20or%20example%20available%20to%20communicate%20with%20an%20I2C%20target%2C%20this%20feature%20can%20be%20helpful%20to%20test%20out%20the%20communication.%26nbsp%3B%20Through%20the%20shell%2C%20I2C%20controllers%20can%20scan%20for%20targets%20and%20send%20read%2Fwrite%20commands%20to%20them.%26nbsp%3B%20Golioth%20shared%20this%20great%20%3CA%20href%3D%22https%3A%2F%2Fblog.golioth.io%2Fhow-to-use-zephyr-shell-for-interactive-prototyping-with-i2c-sensors%2F%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Eblog%20on%20i2c_shell%3C%2FA%3E%20with%20all%20the%20details.%26nbsp%3B%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId--1004686187%22%20id%3D%22toc-hId--946535186%22%3EInter-Integrated%20Circuit%20Sound%20(I2S)%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3EThe%20I2S%20drivers%20are%20tested%20using%20Zephyr%E2%80%99s%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Ftree%2Fmain%2Ftests%2Fdrivers%2Fi2s%2Fi2s_speed%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Ei2s_speed%20test%3C%2FA%3E.%26nbsp%3B%20That%20is%20a%20loopback%20test%2C%20and%20some%20boards%20require%20changes%20to%20connect%20the%20signals%20for%20the%20test%20to%20pass%2C%20see%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Ftree%2Fmain%2Ftests%2Fdrivers%2Fi2s%2Fi2s_speed%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Ereadme%3C%2FA%3E.%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId-1482826646%22%20id%3D%22toc-hId-1540977647%22%3ENetworking%3C%2FH2%3E%0A%3CP%3Eincludes%20Ethernet%3C%2FP%3E%0A%3CUL%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F72760%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EMIMXRT1170-EVK%20Zephyr%20Network%20Performance%3C%2FA%3E%3C%2FLI%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project-Knowledge-Base%2FZephyr-networking-stack-on-i-MX-RT1170-Cortex-M4-secondary-core%2Fta-p%2F2159461%22%20target%3D%22_self%22%3E%3CSPAN%3EZephyr%20networking%20stack%20on%20i.MX%20RT1170%20Cortex-M4%20secondary%20core%3C%2FSPAN%3E%3C%2FA%3E%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId--324627817%22%20id%3D%22toc-hId--266476816%22%3ESerial%20Peripheral%20Interface%20(SPI)%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3EThe%20SPI%20driver%20is%20tested%20with%20Zephyr%E2%80%99s%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Ftree%2Fmain%2Ftests%2Fdrivers%2Fspi%2Fspi_loopback%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Espi_loopback%20test%3C%2FA%3E.%26nbsp%3B%20This%20test%20is%20also%20a%20good%20reference%20for%20the%20options%20to%20place%20DMA%20buffers%20in%20non-cacheable%20memory%2C%20see%20DMA%20above.%3C%2FLI%3E%0A%3CLI%3EWith%20Zephyr%E2%80%99s%20SPI%20driver%2C%20the%20SPI%20Controller%20can%20drive%20the%20chip%20select%20signal%20using%20the%20hardware%20peripheral%20or%20by%20software%20in%20the%20driver%20using%20a%20GPIO.%26nbsp%3B%20To%20learn%20more%2C%20see%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F81264%23discussioncomment-11311957%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EHardware%20chip%20select%20vs%20GPIO%3C%2FA%3E.%26nbsp%3B%20There%20are%20some%20simple%20SPI%20examples%20showing%20this%2C%20see%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F77999%23discussioncomment-10629915%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ELPSPI%20hardware%20chip%20select%20example%3C%2FA%3E%2C%20and%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F81264%23discussioncomment-11311957%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ELPSPI%20GPIO%20chip%20select%20example%3C%2FA%3E.%3C%2FLI%3E%0A%3CLI%3EThe%20SPI%20timing%20parameters%20can%20be%20configured%20in%20devicetree%2C%20see%20the%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fdiscussions%2F77999%23discussioncomment-10629915%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3ELPSPI%20timing%20parameter%20example%3C%2FA%3E.%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CH2%20id%3D%22toc-hId--2132082280%22%20id%3D%22toc-hId--2073931279%22%3EUniversal%20Serial%20Bus%20(USB)%3C%2FH2%3E%0A%3CUL%3E%0A%3CLI%3EUSB%20Host%0A%3CUL%3E%0A%3CLI%3EAs%20of%2012%2F19%2F2025%3A%20USB%20Host%20support%20in%20Zephyr%20is%20very%20limited%2C%20and%20there%20is%20on-going%20work%20to%20enable%20more.%26nbsp%3B%20This%20%3CA%20href%3D%22https%3A%2F%2Fgithub.com%2Fzephyrproject-rtos%2Fzephyr%2Fissues%2F95661%22%20target%3D%22_self%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Etracker%20ticket%3C%2FA%3E%20details%20the%20current%20status%20and%20plans%20for%20USB%20Host%20support.%26nbsp%3B%26nbsp%3B%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3C%2FLI%3E%0A%3CLI%3EUSB%20Device%20is%20supported%2C%20and%20Zephyr%20provides%20several%20%3CA%20href%3D%22https%3A%2F%2Fdocs.zephyrproject.org%2Flatest%2Fsamples%2Fsubsys%2Fusb%2Fusb.html%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3Esample%20applications%3C%2FA%3E%3C%2FLI%3E%0A%3CLI%3E%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project-Knowledge-Base%2FZephyr-networking-IP-over-USB-CDC-NCM%2Fta-p%2F2171182%22%20target%3D%22_self%22%3ENetworking%20IP%20over%20USB%20CDC%20NCM%3C%2FA%3E%3C%2FLI%3E%0A%3C%2FUL%3E%0A%3CBR%20%2F%3E%0A%3CP%3EReturn%20to%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FZephyr-Project-Knowledge-Base%2FZephyr-Support-Resources%2Fta-p%2F2008548%22%20target%3D%22_blank%22%3EZephyr%20Knowledge%20Hub%3C%2FA%3E%3C%2FP%3E%0A%3C%2FLINGO-BODY%3E
No ratings
Version history
Last update:
‎12-19-2025 08:44 AM
Updated by: