Zephyr resources for Peripherals and drivers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Zephyr resources for Peripherals and drivers

Zephyr resources for Peripherals and drivers

If you have any questions or issues related to these resources, please Ask a new question, and the NXP support team can address it there.

One of the popular reasons developers choose Zephyr is the large offering of drivers and peripheral support.  The best place to look for the latest drivers and features supported on a hardware platform, is on the board’s documentation page.  For example, this Supported Features table lists the latest support for the FRDM-MCXN947 board.  Here are the links to these pages for all the boards with Zephyr support.

NXP’s Hardware Abstraction Layer (HAL) is based on the MCUXpresso SDK drivers.  To learn more, see the blog Zephyr Software Code Reuse with NXP MCUXpresso SDK.  Most users want to use the Zephyr driver APIs in their application for portability.  But if a Zephyr driver is not supported on a platform, or if there is no Zephyr driver for a hardware peripheral, another option is Using MCUXpresso SDK drivers in Zephyr app.

Peripheral Clocks: Most peripheral clocks are enabled in SOC or board source files, see Clock Configuration in Zephyr.  One common issue Zephyr users have when enabling or adding a peripheral instance on their board, is that instance is not clocked properly.  Below are some helpful resources for specific peripherals and drivers:

Accelerators and Coprocessors

Analog to Digital Converter (ADC)

Displays

  • Most displays are enabled in Zephyr as shields, which are add-on hardware modules.  See Zephyr’s list of shields.
  • Typically a board page will document a display shield it has been tested with.  For example, the FRDM-MCXN947 board page includes the LCD_PAR_S035 display shield.
  • The shield page gives instructions how to include that shield in the build, and add to the application.  For example, see the LCD_PAR_S035 shield page.  If building with VS Code, see the CMake wiki
  • Zephyr has a couple samples that use displays, including the display driver sample and the LVGL demo.

Direct Memory Access (DMA)

  • When using a DMA, be aware of cache coherency, and make sure buffers accessed by DMA are not in cacheable memory.  This includes when using other drivers that use DMA, like I2S, SPI, UART, etc..  A good reference for placing buffers in non-cacheable memory is the spi_loopback test.

Inter-Integrated Circuit Sound (I2S)

  • The I2S drivers are tested using Zephyr’s i2s_speed test.  That is a loopback test, and some boards require changes to connect the signals for the test to pass, see the readme.

Networking

includes Ethernet

Serial Peripheral Interface (SPI)

Universal Serial Bus (USB)

  • USB Host
    • As of 12/5/2024: Zephyr does not support USB Host today.  The USB maintainer has this RFC tracker for the planned enhancement to add USB Host support.  But today, there is only experimental Host APIs.  The USB Host stack has not been implemented yet, nor are any USB classes supported yet.  Progress and status can be tracked by following this RFC. 
  • USB Device is supported, and Zephyr provides several sample applications
  • Networking IP over USB CDC NCM

 

Return to Zephyr Knowledge Hub

无评分
版本历史
最后更新:
2 周之前
更新人: