zigbee broadcast

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

zigbee broadcast

2,414 Views
weisheng
Contributor III

Hi all,

      I got a problem in end device to receive broadcast.

      There is a coordinator and 15 end devices in a network, I need to send broadcast from coordinator to end device, but just the first seven end devices can receive the message, and always can,the other devices can not receive the broadcast all the time. The end device polling message every one second.

      

      I want to know why not all the end device can receive broadcast successfully?

      Thanks in advance!

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,297 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Wei,

What is the application note that you are working on?

Do you have the sniffer log of this issue?

Do you have only end devices?

Regards,

Mario

0 Kudos
Reply

2,297 Views
weisheng
Contributor III

Hi Mario,

What is the application note that you are working on?

I use "JN-AN-1217-Zigbee-3-0-Base-Device" project, and JN-SW-4170-Zigbee-3.0-v1518 SDK

Do you have the sniffer log of this issue?

I do not got the sniffer log.

Do you have only end devices?

there is only coordinator and end device.

0 Kudos
Reply

2,297 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Wei,

We provide the sniffer example in the SDK folder.

C:\NXP\bstudio_nxp\sdk\JN-SW-4170\Tools\JennicSniffer

The sniffer supports Ubiqua software. The sniffer will show what is happening with the end devices, It is a broadcast and the other devices are receiving the data.

Then, could you please update the SDK to the last version that we launched.

JN-SW-4170 Version 1614

Zigbee 3.0

Regards,

Mario

0 Kudos
Reply