why i cannot upgrade the PN5180's firmware?
[2022.01.27 20:01:33]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while writing to COM6[2022.01.27 20:01:33]:ERROR:BoardConnectionViewModel:Secure Firmware Upgrade Failed. Status=BAL,IO_TIMEOUT
已解决! 转到解答。
the bin file run in LPC1769 mcu is C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin
and i can read the M1 card's UUID.
在原帖中查看解决方案
AN11744 is for PNEV5180 board, as below. but it is different from yours
my PN5180 board just copy from PNEV5180!!! the communicate connection with PN5180 is the same to
NXP.s PNEV5180!!!
how to use BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin file ?
how to burn the bin file to LPC1769?
Please use GUI Flash tool in MCUXpresso IDE. see below picture
can i use Flash Magic to burn the LPC1769 MCU?
but the Flash Magic need use hex format file. how to convert the bin file to hex file ?
i have not install MCUXpresso IDE. and i have not the LPClink JTAG tool.
what can i do ?
MCUXpresso IDE can be downloaded from below link
https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-i...