what Input multiplexing function mean in QN908X?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what Input multiplexing function mean in QN908X?

1,345 Views
wdliming
Contributor I

when i read the Input multiplexing function in QN908X  doc, but i can not understand what that module can do? which circumstances that will use this funtion?

can anyone to explain it more easy? 

thanks a lot!

Labels (1)
0 Kudos
Reply
1 Reply

1,296 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

I believe you are referring to chapter 9 in the user manual, is that right?

If you do, that chapter just explains that you will need to use the input multiplexing in order to route an interruption to a pin or when using the pin as a DMA trigger.

Hopefully that it's simpler and help you a little more. 

Regards

0 Kudos
Reply