vAHI_SwReset() API, which will trigger a Leave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vAHI_SwReset() API, which will trigger a Leave

1,601件の閲覧回数
zigbee1
Contributor III

We are currently maintaining a  Zigbee controller out of JN5169.
We are using the JN-SW-4170 SDK.
We have of course a good understanding of JN-AN-1216
Application Note: JN-AN-1216 ZigBee 3.0 IoT Control Bridge,
as well as the JN-UG-3113 User Guide section B.5

We detect a strange behaviour after calling vAHI_SwReset(), indeed after such call any devices which is in the Child Table receive from the Controller a Leave message

Is there an expected behaviour ?

Is there a configuration to disable such behaviour and prevent the Leave message to be issued ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,581件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

vAHI_SwReset. This reset has the same effect as pulling the external RESETN line low and is likely to result in the loss of the contents of on-chip RAM

Do you have a sniffer log about this behavior?

Regards,

Mario

0 件の賞賛
返信