use COM TOOLS to debug control-bridge project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use COM TOOLS to debug control-bridge project

3,227件の閲覧回数
18916628579
Contributor I

HI    

       Use FRDM-KW41 board debug  ZigBee-3-0-ControlBridge project. NXP Test Tool 12/ZGWUI will work well,

       But I want to use COM TOOLS to debug ,The output is garbled/ with 115200(see the attachment). so if I want to use COM TOOLS to debug ,where need set in project frdmkw41z_wireless_examples_zigbee_3_0_control_bridge_freertos.

thanks

br

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,157件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liu,

Please look at the Application NoteZigBee 3.0 IoT Control Bridge.

"SDK_SDK_2.2_FRDM-KW41Z\docs\wireless\Zigbee\Application Notes\AN12063-MKW41Z-AN-ZigBee-3-0-ControlBridge.pdf".

Appendix A: Serial Protocol

pastedImage_3.png

pastedImage_2.png

Please let me know if you have issues with the commands.

Regards,

Mario

0 件の賞賛
返信

3,157件の閲覧回数
18916628579
Contributor I

hi mario:

thanks

br

jim

0 件の賞賛
返信