u16SizeOfKeyDescriptorTable is wrong

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

u16SizeOfKeyDescriptorTable is wrong

1,462 次查看
vishal_zadafiy1
Contributor I

Hi all
I am using JN-AN-1216-Zigbee-3-0-IoT-ControlBridge Application and JN-SW-4270 SDK for JN-5179.

I had set Trust center table size and Aps key Table size is 70  on config file but still i am getting the 

tsAplAib->psAplDeviceKeyPairTable->u16SizeOfKeyDescriptorTable is 1 only.

Also i share screen for same.

Is it correct ? if not how to resolve it?

标签 (1)
0 项奖励
回复
1 回复

1,393 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vishal,

The zps_gen.c/h  These are generated files. Do not edit.

Be sure that you are modifying the correct zpscfg file. The jn-an-1216 provides 4 different files and depending on the example that you have active it will be selected. You can modify this in the makefile.

I compile the Zigbee Node Control Bridge Coordinator for the JN5199

It is taking this file ZigbeeNodeControlBridgeCoordinator_GP_Proxy.zpscfg

I am not sure if you want to work with the Preconfigured key, but it is no longer supported feature.User can use AddReplaceLinkKey and SetInitialSecurityState instead.

Regards,

Mario

0 项奖励
回复